43 #ifndef __SYSTICK_UTILS_H__ 44 #define __SYSTICK_UTILS_H__ 95 #endif // __SYSTICK_UTILS_H__ void BOARD_SystickStart(int32_t *pStart)
Function to Record the Start systick.
uint32_t BOARD_SystickElapsedTime_us(int32_t *pStart)
Function to compute the Elapsed Time.
void BOARD_SystickEnable(void)
Function to enable systicks framework.
int32_t BOARD_SystickElapsedTicks(int32_t *pStart)
Function to compute the Elapsed systicks.
void BOARD_DELAY_ms(uint32_t delay_ms)
Function to insert delays.