14 #define MMA9553_HDR_SIZE  (4)    17 #define VERSION_INFO_SIZE (12)    20 #define STANDBY_REG_SIZE (4)    23 #define MMA9553_XYZ_DATA_OFFSET (26)    26 #define MMA9553_I2C_ADDRESS (0x4C) const uint8_t SetAFEPriority_for3Hz[5]
 
const uint8_t SetAFEPriority_for7Hz[5]
 
const uint8_t SetMBoxPriority_for244Hz[5]
 
const uint8_t SetMBoxPriority_for15Hz[5]
 
const uint8_t SetSampleRate_7Hz[5]
 
const uint8_t SetSampleRate_30Hz[5]
 
const uint8_t SetLegacyMode[5]
Set Sensor to Legacy (free running) Mode Command. 
 
const uint8_t SetSampleRate_61Hz[5]
 
const uint8_t SetMBoxPriority_for7Hz[5]
 
const uint8_t SetSampleRate_3Hz[5]
 
const uint8_t ReadPedometerData[4]
Command to Read Pedometer Data. 
 
const uint8_t SetAFEPriority_for61Hz[5]
 
const uint8_t SetFSRange_8g[5]
 
const uint8_t SetSampleRate_488Hz[5]
Sample Rate Commands. 
 
const uint8_t SetMBoxPriority_for61Hz[5]
 
const uint8_t SetFSRange_2g[5]
Full-Scale Range Selections. 
 
const uint8_t SetMBoxPriority_for488Hz[5]
MBox Priority Commands. 
 
const uint8_t ResetApplication[5]
Command to reset all applications of the sensor. 
 
const uint8_t SetAFEPriority_for30Hz[5]
 
const uint8_t SetSampleRate_244Hz[5]
 
const uint8_t SetMBoxPriority_for3Hz[5]
 
const uint8_t SetAFEPriority_for224Hz[5]
 
const uint8_t ReadVersionInfo[4]
The Read Version Info Command. 
 
const uint8_t SetFSRange_4g[5]
 
const uint8_t WakeApplication[5]
Set sensor to Wake Mode Command. 
 
const uint8_t SetMBoxPriority_for30Hz[5]
 
const uint8_t SetAFEPriority_for488Hz[5]
AFE Priority Commands. 
 
const uint8_t SetAFEPriority_for122Hz[5]
 
const uint8_t SetLegacyIntMode[5]
Set Sensor to Legacy Mode with INT_O interrupt on completion of the AFE sampling. ...
 
const uint8_t MBoxQRDataXYZ[16]
Configure MBOX for QR Data and XYZ Axes Command. 
 
const uint8_t SetSampleRate_15Hz[5]
 
const uint8_t SetSampleRate_122Hz[5]
 
const uint8_t SetAFEPriority_for15Hz[5]
 
const uint8_t SetMBoxPriority_for122Hz[5]