16 #ifndef __ISSDK_HAL_H__ 17 #define __ISSDK_HAL_H__ 19 #include "fsl_lpspi_cmsis.h" 20 #include "fsl_lpi2c_cmsis.h" 21 #include "fsl_lpuart_cmsis.h" 26 #endif // __ISSDK_HAL_H__ The frdm-stba-pa7250_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-ke1...
The frdm_ke15z.h file defines GPIO pin mappings for FRDM-KE15Z board.