ISSDK  1.8
IoT Sensing Software Development Kit
freemaster_cfg.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2007-2015 Freescale Semiconductor, Inc.
3  * Copyright 2018-2019 NXP
4  *
5  * SPDX-License-Identifier: BSD-3-Clause
6  *
7  * FreeMASTER Communication Driver - User Configuration File
8  */
9 
10 #ifndef __FREEMASTER_CFG_H
11 #define __FREEMASTER_CFG_H
12 
13 ////////////////////////////////////////////////////////////////////////////////
14 // Definitions
15 ////////////////////////////////////////////////////////////////////////////////
16 
17 #define FMSTR_PLATFORM_CORTEX_M 1 /* Cortex-M platform (see freemaster.h for list of all supported platforms) */
18 
19 //! Set the demo application configuration
20 #define FMSTR_DEMO_ENOUGH_ROM 1 /* Platform has enough ROM to show most of the FreeMASTER features */
21 #define FMSTR_DEMO_LARGE_ROM 1 /* Platform has large ROM enough to store the extended data structures used in FreeMASTER demo */
22 #define FMSTR_DEMO_SUPPORT_I64 1 /* support for long long type */
23 #define FMSTR_DEMO_SUPPORT_FLT 1 /* support for float type */
24 #define FMSTR_DEMO_SUPPORT_DBL 0 /* support for double type */
25 
26 
27 //! Enable/Disable FreeMASTER support as a whole
28 #define FMSTR_DISABLE 0 // To disable all FreeMASTER functionalities
29 
30 //! Select interrupt or poll-driven serial communication
31 #define FMSTR_LONG_INTR 1 // Complete message processing in interrupt
32 #define FMSTR_SHORT_INTR 0 // Queuing done in interrupt
33 #define FMSTR_POLL_DRIVEN 0 // No interrupt needed, polling only
34 
35 // List of standard FreeMASTER transports and their low-level drivers. See more options in src/drivers.
36 // FMSTR_SERIAL - Standard serial transport protocol (Used by various types of UART peripherals as USB CDC implementation)
37 // FMSTR_SERIAL_MCUX_UART - MCUXSDK driver for UART peripheral
38 // FMSTR_SERIAL_MCUX_LPUART - MCUXSDK driver for LPUART peripheral
39 // FMSTR_SERIAL_MCUX_USART - MCUXSDK driver for USART peripheral
40 // FMSTR_SERIAL_MCUX_MINIUSART -MCUXSDK driver for MINIUSART peripheral
41 // FMSTR_SERIAL_MCUX_USB - MCUXSDK driver for USB peripheral with CDC class
42 // FMSTR_CAN - Standard CAN transport protocol (Used by various types of CAN peripherals)
43 // FMSTR_CAN_MCUX_FLEXCAN - MCUXSDK driver for FlexCAN peripheral
44 // FMSTR_CAN_MCUX_MCAN - MCUXSDK driver for MCAN peripheral
45 // FMSTR_CAN_MCUX_MSCAN - MCUXSDK driver for msCAN peripheral
46 // FMSTR_PDBDM - Packet Driven BDM (direct memory access via JTAG, SWD or BDM debug probes). No low-level driver used.
47 
48 //! Select communication interface
49 #define FMSTR_TRANSPORT FMSTR_SERIAL // Use serial transport layer */
50 #define FMSTR_SERIAL_DRV FMSTR_SERIAL_MCUX_UART // Use serial driver for UART */
51 
52 //! Define communication interface base address or leave undefined for runtime setting
53 // #undef FMSTR_SERIAL_BASE // Serial base will be assigned in runtime (when FMSTR_USE_UART)
54 // #undef FMSTR_CAN_BASE // CAN base will be assigned in runtime (when FMSTR_USE_FLEXCAN)
55 
56 //! FlexCAN-specific, communication message buffers
57 #define FMSTR_FLEXCAN_TXMB 0
58 #define FMSTR_FLEXCAN_RXMB 1
59 
60 //! Input/output communication buffer size
61 #define FMSTR_COMM_BUFFER_SIZE 0 // Set to 0 for "automatic"
62 
63 //! Receive FIFO queue size (use with FMSTR_SHORT_INTR only)
64 #define FMSTR_COMM_RQUEUE_SIZE 32 // Set to 0 for "default"
65 
66 //! Support for Application Commands
67 #define FMSTR_USE_APPCMD 1 // Enable/disable App.Commands support
68 #define FMSTR_APPCMD_BUFF_SIZE 32 // App.Command data buffer size
69 #define FMSTR_MAX_APPCMD_CALLS 4 // How many app.cmd callbacks? (0=disable)
70 
71 //! Oscilloscope support
72 #define FMSTR_USE_SCOPE 2 // Specify number of supported oscilloscopes
73 #define FMSTR_MAX_SCOPE_VARS 8 // Specify maximum number of scope variables per one oscilloscope
74 
75 //! Recorder support
76 #define FMSTR_USE_RECORDER 2 // Specify number of supported recorders
77 
78 //! Built-in recorder buffer
79 #define FMSTR_REC_BUFF_SIZE 1024 // Built-in buffer size of recorder #0. Set to 0 to use runtime settings.
80 
81 //! Recorder time base, specifies how often the recorder is called in the user app.
82 #define FMSTR_REC_TIMEBASE FMSTR_REC_BASE_MILLISEC(0) // 0 = "unknown"
83 #define FMSTR_REC_FLOAT_TRIG 1 // Enable/disable floating point triggering
84 
85 // Target-side address translation (TSA)
86 #define FMSTR_USE_TSA 1 // Enable TSA functionality
87 #define FMSTR_USE_TSA_INROM 1 // TSA tables declared as const (put to ROM)
88 #define FMSTR_USE_TSA_SAFETY 1 // Enable/Disable TSA memory protection
89 #define FMSTR_USE_TSA_DYNAMIC 1 // Enable/Disable TSA entries to be added also in runtime
90 
91 // Pipes as data streaming over FreeMASTER protocol
92 #define FMSTR_USE_PIPES 3 // Specify number of supported pipe objects
93 
94 // Enable/Disable read/write memory commands
95 #define FMSTR_USE_READMEM 1 // Enable read memory commands
96 #define FMSTR_USE_WRITEMEM 1 // Enable write memory commands
97 #define FMSTR_USE_WRITEMEMMASK 1 // Enable write memory bits commands
98 
99 // Define password for access levels to protect them. AVOID SHORT PASSWORDS in production version.
100 // Passwords should be at least 20 characters long to prevent dictionary attacks.
101 // #define FMSTR_RESTRICTED_ACCESS_R_PASSWORD "r" // Read-only access level password. Let undefined when no password is required.
102 // #define FMSTR_RESTRICTED_ACCESS_RW_PASSWORD "rw" // Write access level password. Let undefined to set the same as for read-only access level.
103 // #define FMSTR_RESTRICTED_ACCESS_RWF_PASSWORD "rwf" // Flash access level password. Let undefined to set the same as for write access level.
104 
105 // Storing cleartext passwords in Flash memory is not safe, consider storing their SHA1 hash instead
106 // Even with this option, the hash must be generated from reasonably complex password to prevent dictionary attack.
107 #define FMSTR_USE_HASHED_PASSWORDS 0 // When non-zero, the passwords above are specified as a pointer to 20-byte SHA1 hash of password text
108 
109 #endif /* __FREEMASTER_CFG_H */
110 
111 ////////////////////////////////////////////////////////////////////////////////
112 // EOF
113 ////////////////////////////////////////////////////////////////////////////////