ISSDK
1.8
IoT Sensing Software Development Kit
driverexamples
fxls8974cf
freemaster_cfg.h
Go to the documentation of this file.
1
/*
2
* Copyright (c) 2007-2015 Freescale Semiconductor, Inc.
3
* Copyright 2018-2019 NXP
4
*
5
* SPDX-License-Identifier: BSD-3-Clause
6
*
7
* FreeMASTER Communication Driver - User Configuration File
8
*/
9
10
#ifndef __FREEMASTER_CFG_H
11
#define __FREEMASTER_CFG_H
12
13
////////////////////////////////////////////////////////////////////////////////
14
// Definitions
15
////////////////////////////////////////////////////////////////////////////////
16
17
#define FMSTR_PLATFORM_CORTEX_M 1
/* Cortex-M platform (see freemaster.h for list of all supported platforms) */
18
19
//! Set the demo application configuration
20
#define FMSTR_DEMO_ENOUGH_ROM 1
/* Platform has enough ROM to show most of the FreeMASTER features */
21
#define FMSTR_DEMO_LARGE_ROM 1
/* Platform has large ROM enough to store the extended data structures used in FreeMASTER demo */
22
#define FMSTR_DEMO_SUPPORT_I64 1
/* support for long long type */
23
#define FMSTR_DEMO_SUPPORT_FLT 1
/* support for float type */
24
#define FMSTR_DEMO_SUPPORT_DBL 0
/* support for double type */
25
26
27
//! Enable/Disable FreeMASTER support as a whole
28
#define FMSTR_DISABLE 0 // To disable all FreeMASTER functionalities
29
30
//! Select interrupt or poll-driven serial communication
31
#define FMSTR_LONG_INTR 1 // Complete message processing in interrupt
32
#define FMSTR_SHORT_INTR 0 // Queuing done in interrupt
33
#define FMSTR_POLL_DRIVEN 0 // No interrupt needed, polling only
34
35
// List of standard FreeMASTER transports and their low-level drivers. See more options in src/drivers.
36
// FMSTR_SERIAL - Standard serial transport protocol (Used by various types of UART peripherals as USB CDC implementation)
37
// FMSTR_SERIAL_MCUX_UART - MCUXSDK driver for UART peripheral
38
// FMSTR_SERIAL_MCUX_LPUART - MCUXSDK driver for LPUART peripheral
39
// FMSTR_SERIAL_MCUX_USART - MCUXSDK driver for USART peripheral
40
// FMSTR_SERIAL_MCUX_MINIUSART -MCUXSDK driver for MINIUSART peripheral
41
// FMSTR_SERIAL_MCUX_USB - MCUXSDK driver for USB peripheral with CDC class
42
// FMSTR_CAN - Standard CAN transport protocol (Used by various types of CAN peripherals)
43
// FMSTR_CAN_MCUX_FLEXCAN - MCUXSDK driver for FlexCAN peripheral
44
// FMSTR_CAN_MCUX_MCAN - MCUXSDK driver for MCAN peripheral
45
// FMSTR_CAN_MCUX_MSCAN - MCUXSDK driver for msCAN peripheral
46
// FMSTR_PDBDM - Packet Driven BDM (direct memory access via JTAG, SWD or BDM debug probes). No low-level driver used.
47
48
//! Select communication interface
49
#define FMSTR_TRANSPORT FMSTR_SERIAL // Use serial transport layer */
50
#define FMSTR_SERIAL_DRV FMSTR_SERIAL_MCUX_UART // Use serial driver for UART */
51
52
//! Define communication interface base address or leave undefined for runtime setting
53
// #undef FMSTR_SERIAL_BASE // Serial base will be assigned in runtime (when FMSTR_USE_UART)
54
// #undef FMSTR_CAN_BASE // CAN base will be assigned in runtime (when FMSTR_USE_FLEXCAN)
55
56
//! FlexCAN-specific, communication message buffers
57
#define FMSTR_FLEXCAN_TXMB 0
58
#define FMSTR_FLEXCAN_RXMB 1
59
60
//! Input/output communication buffer size
61
#define FMSTR_COMM_BUFFER_SIZE 0 // Set to 0 for "automatic"
62
63
//! Receive FIFO queue size (use with FMSTR_SHORT_INTR only)
64
#define FMSTR_COMM_RQUEUE_SIZE 32 // Set to 0 for "default"
65
66
//! Support for Application Commands
67
#define FMSTR_USE_APPCMD 1 // Enable/disable App.Commands support
68
#define FMSTR_APPCMD_BUFF_SIZE 32 // App.Command data buffer size
69
#define FMSTR_MAX_APPCMD_CALLS 4 // How many app.cmd callbacks? (0=disable)
70
71
//! Oscilloscope support
72
#define FMSTR_USE_SCOPE 2 // Specify number of supported oscilloscopes
73
#define FMSTR_MAX_SCOPE_VARS 8 // Specify maximum number of scope variables per one oscilloscope
74
75
//! Recorder support
76
#define FMSTR_USE_RECORDER 2 // Specify number of supported recorders
77
78
//! Built-in recorder buffer
79
#define FMSTR_REC_BUFF_SIZE 1024 // Built-in buffer size of recorder #0. Set to 0 to use runtime settings.
80
81
//! Recorder time base, specifies how often the recorder is called in the user app.
82
#define FMSTR_REC_TIMEBASE FMSTR_REC_BASE_MILLISEC(0) // 0 = "unknown"
83
#define FMSTR_REC_FLOAT_TRIG 1 // Enable/disable floating point triggering
84
85
// Target-side address translation (TSA)
86
#define FMSTR_USE_TSA 1 // Enable TSA functionality
87
#define FMSTR_USE_TSA_INROM 1 // TSA tables declared as const (put to ROM)
88
#define FMSTR_USE_TSA_SAFETY 1 // Enable/Disable TSA memory protection
89
#define FMSTR_USE_TSA_DYNAMIC 1 // Enable/Disable TSA entries to be added also in runtime
90
91
// Pipes as data streaming over FreeMASTER protocol
92
#define FMSTR_USE_PIPES 3 // Specify number of supported pipe objects
93
94
// Enable/Disable read/write memory commands
95
#define FMSTR_USE_READMEM 1 // Enable read memory commands
96
#define FMSTR_USE_WRITEMEM 1 // Enable write memory commands
97
#define FMSTR_USE_WRITEMEMMASK 1 // Enable write memory bits commands
98
99
// Define password for access levels to protect them. AVOID SHORT PASSWORDS in production version.
100
// Passwords should be at least 20 characters long to prevent dictionary attacks.
101
// #define FMSTR_RESTRICTED_ACCESS_R_PASSWORD "r" // Read-only access level password. Let undefined when no password is required.
102
// #define FMSTR_RESTRICTED_ACCESS_RW_PASSWORD "rw" // Write access level password. Let undefined to set the same as for read-only access level.
103
// #define FMSTR_RESTRICTED_ACCESS_RWF_PASSWORD "rwf" // Flash access level password. Let undefined to set the same as for write access level.
104
105
// Storing cleartext passwords in Flash memory is not safe, consider storing their SHA1 hash instead
106
// Even with this option, the hash must be generated from reasonably complex password to prevent dictionary attack.
107
#define FMSTR_USE_HASHED_PASSWORDS 0 // When non-zero, the passwords above are specified as a pointer to 20-byte SHA1 hash of password text
108
109
#endif
/* __FREEMASTER_CFG_H */
110
111
////////////////////////////////////////////////////////////////////////////////
112
// EOF
113
////////////////////////////////////////////////////////////////////////////////
© Copyright 2016-2020 NXP. All Rights Reserved.