![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral UART driver for the Universal Synchronous Receiver/Transmitter (USART) module of MCUXpresso SDK devices. Driver does not support synchronous mode.
The USART driver includes two parts: functional APIs and transactional APIs.
Functional APIs are used for USART initialization/configuration/operation for the purpose of optimization/customization. Using the functional API requires the knowledge of the USART peripheral and know how to organize functional APIs to meet the application requirements. All functional API use the peripheral base address as the first parameter. USART functional operation groups provide the functional APIs set.
Transactional APIs can be used to enable the peripheral quickly and in the application if the code size and performance of transactional APIs can satisfy the requirements. If the code size and performance are critical requirements, see the transactional API implementation and write custom code. All transactional APIs use the usart_handle_t as the second parameter. Initialize the handle by calling the USART_TransferCreateHandle() API.
Transactional APIs support asynchronous transfer, which means that the functions USART_TransferSendNonBlocking() and USART_TransferReceiveNonBlocking() set up an interrupt for data transfer. When the transfer completes, the upper layer is notified through a callback function with the kStatus_USART_TxIdle and kStatus_USART_RxIdle.
Transactional receive APIs support the ring buffer. Prepare the memory for the ring buffer and pass in the start address and size while calling the USART_TransferCreateHandle(). If passing NULL, the ring buffer feature is disabled. When the ring buffer is enabled, the received data is saved to the ring buffer in the background. The USART_TransferReceiveNonBlocking() function first gets data from the ring buffer. If the ring buffer does not have enough data, the function first returns the data in the ring buffer and then saves the received data to user memory. When all data is received, the upper layer is informed through a callback with the kStatus_USART_RxIdle.
If the receive ring buffer is full, the upper layer is informed through a callback with the kStatus_USART_RxRingBufferOverrun. In the callback function, the upper layer reads data out from the ring buffer. If not, the oldest data is overwritten by the new data.
The ring buffer size is specified when creating the handle. Note that one byte is reserved for the ring buffer maintenance. When creating handle using the following code:
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/usart In this example, the buffer size is 32, but only 31 bytes are used for saving data.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/usart
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/usart
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/usart
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/usart
Modules | |
| USART CMSIS Driver | |
| USART DMA Driver | |
| USART Driver | |
| USART FreeRTOS Driver | |