AWS Account setup
- Setup your AWS account for OTA: https://docs.aws.amazon.com/freertos/latest/userguide/ota-prereqs.html
System Setup
- This script currently uses Python 3, please make sure you have the latest python installed: https://www.python.org/downloads/.
- Install the required python libraries:
pip3 install pyopenssl pyserial junit-xml boto3
- Install the AWS CLI: https://aws.amazon.com/cli/
- Configure the AWS CLI from the terminal:
aws configure
Board Configuration Setup
The test scripts need information unique to your board and your AWS account. This is contained in a board.json.
- See board.json in the same directory as this README for information on each field. Create one or more for each board you wish to run tests on. Some items are pre-filled, please verify the configuration is sufficient to your needs.
- Some tests are designed to check that un-trusted certificates do not work. If you do not want to generate your own throw-away certificate/key pairs, example certificates are provided, for signing schemes using RSA SHA256 and ECDSA SHA256, under the 'credentials' directory. The names of the files indicate the signing algorithm. Import the certificates with the algorithm applicable to your device into AWS Certificate Manager. Use the resulting ARN for the
"aws_untrusted_signer_certificate_arn" board config value.
Running the tests
- Run all of the tests on board specified in board.json:
python ota_e2e.py --board-configs board.json
- Run all of the tests on directory of board configurations:
python ota_e2e.py --board-config-dir C:/example_dir/board_configs/
- Run only the specified tests:
python ota_e2e.py --board-configs board.json --tests OtaTestGreaterVersion The names of the available tests are pre-filled in board.json under the "supported_tests" field.
- More options specified in –help:
python ota_e2e.py --help