![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
semphr. h
xSemaphoreTake(
SemaphoreHandle_t xSemaphore,
TickType_t xBlockTime
)Macro to obtain a semaphore. The semaphore must have previously been created with a call to xSemaphoreCreateBinary(), xSemaphoreCreateMutex() or xSemaphoreCreateCounting().
| xSemaphore | A handle to the semaphore being taken - obtained when the semaphore was created. |
| xBlockTime | The time in ticks to wait for the semaphore to become available. The macro portTICK_PERIOD_MS can be used to convert this to a real time. A block time of zero can be used to poll the semaphore. A block time of portMAX_DELAY can be used to block indefinitely (provided INCLUDE_vTaskSuspend is set to 1 in FreeRTOSConfig.h). |
Example usage:
SemaphoreHandle_t xSemaphore = NULL;
A task that creates a semaphore.
void vATask( void * pvParameters )
{
Create the semaphore to guard a shared resource.
xSemaphore = xSemaphoreCreateBinary();
}A task that uses the semaphore.
void vAnotherTask( void * pvParameters )
{
... Do other things.
if( xSemaphore != NULL )
{
See if we can obtain the semaphore. If the semaphore is not available
wait 10 ticks to see if it becomes free.
if( xSemaphoreTake( xSemaphore, ( TickType_t ) 10 ) == pdTRUE )
{
We were able to obtain the semaphore and can now access the
shared resource.
...
We have finished accessing the shared resource. Release the
semaphore.
xSemaphoreGive( xSemaphore );
}
else
{
We could not obtain the semaphore and can therefore not access
the shared resource safely.
}
}
}