![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
task. h
void vTaskResume( TaskHandle_t xTaskToResume );
INCLUDE_vTaskSuspend must be defined as 1 for this function to be available. See the configuration section for more information.
Resumes a suspended task.
A task that has been suspended by one or more calls to vTaskSuspend () will be made available for running again by a single call to vTaskResume ().
| xTaskToResume | Handle to the task being readied. |
Example usage:
void vAFunction( void )
{
TaskHandle_t xHandle;Create a task, storing the handle.
xTaskCreate( vTaskCode, "NAME", STACK_SIZE, NULL, tskIDLE_PRIORITY, &xHandle );...
Use the handle to suspend the created task.
vTaskSuspend( xHandle );...
The created task will not run during this period, unless another task calls vTaskResume( xHandle ).
...
Resume the suspended task ourselves.
vTaskResume( xHandle );The created task will once again get microcontroller processing time in accordance with its priority within the system. }