![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
task. h
UBaseType_t uxTaskPriorityGet( const TaskHandle_t xTask );
INCLUDE_uxTaskPriorityGet must be defined as 1 for this function to be available. See the configuration section for more information.
Obtain the priority of any task.
| xTask | Handle of the task to be queried. Passing a NULL handle results in the priority of the calling task being returned. | 
Example usage:
 void vAFunction( void )
 {
 TaskHandle_t xHandle;Create a task, storing the handle.
     xTaskCreate( vTaskCode, "NAME", STACK_SIZE, NULL, tskIDLE_PRIORITY, &xHandle );...
Use the handle to obtain the priority of the created task.
It was created with tskIDLE_PRIORITY, but may have changed
it itself.
     if( uxTaskPriorityGet( xHandle ) != tskIDLE_PRIORITY )
     {
The task has changed it's priority.
     }...
Is our priority higher than the created task?
     if( uxTaskPriorityGet( xHandle ) < uxTaskPriorityGet( NULL ) )
     {
Our priority (obtained using NULL handle) is higher.
     }
 }