![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
message_buffer.h
MessageBufferHandle_t xMessageBufferCreate( size_t xBufferSizeBytes );
Creates a new message buffer using dynamically allocated memory. See xMessageBufferCreateStatic() for a version that uses statically allocated memory (memory that is allocated at compile time).
configSUPPORT_DYNAMIC_ALLOCATION must be set to 1 or left undefined in FreeRTOSConfig.h for xMessageBufferCreate() to be available.
xBufferSizeBytes | The total number of bytes (not messages) the message buffer will be able to hold at any one time. When a message is written to the message buffer an additional sizeof( size_t ) bytes are also written to store the message's length. sizeof( size_t ) is typically 4 bytes on a 32-bit architecture, so on most 32-bit architectures a 10 byte message will take up 14 bytes of message buffer space. |
Example use:
void vAFunction( void ) { MessageBufferHandle_t xMessageBuffer; const size_t xMessageBufferSizeBytes = 100;// Create a message buffer that can hold 100 bytes. The memory used to hold // both the message buffer structure and the messages themselves is allocated // dynamically. Each message added to the buffer consumes an additional 4 // bytes which are used to hold the lengh of the message. xMessageBuffer = xMessageBufferCreate( xMessageBufferSizeBytes ); if( xMessageBuffer == NULL ) { // There was not enough heap memory space available to create the // message buffer. } else { // The message buffer was created successfully and can now be used. }