MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
xMessageBufferSendFromISR

message_buffer.h

size_t xMessageBufferSendFromISR( MessageBufferHandle_t xMessageBuffer,
                                  const void *pvTxData,
                                  size_t xDataLengthBytes,
                                  BaseType_t *pxHigherPriorityTaskWoken );

   Interrupt safe version of the API function that sends a discrete message to
   the message buffer.  The message can be any length that fits within the
   buffer's free space, and is copied into the buffer.
   ***NOTE***:  Uniquely among FreeRTOS objects, the stream buffer
   implementation (so also the message buffer implementation, as message buffers
   are built on top of stream buffers) assumes there is only one task or
   interrupt that will write to the buffer (the writer), and only one task or
   interrupt that will read from the buffer (the reader).  It is safe for the
   writer and reader to be different tasks or interrupts, but, unlike other
   FreeRTOS objects, it is not safe to have multiple different writers or
   multiple different readers.  If there are to be multiple different writers
   then the application writer must place each call to a writing API function
   (such as xMessageBufferSend()) inside a critical section and set the send
   block time to 0.  Likewise, if there are to be multiple different readers
   then the application writer must place each call to a reading API function
   (such as xMessageBufferRead()) inside a critical section and set the receive
   block time to 0.
   Use xMessageBufferSend() to write to a message buffer from a task.  Use
   xMessageBufferSendFromISR() to write to a message buffer from an interrupt
   service routine (ISR).
   
Parameters
xMessageBufferThe handle of the message buffer to which a message is being sent.
pvTxDataA pointer to the message that is to be copied into the message buffer.
xDataLengthBytesThe length of the message. That is, the number of bytes to copy from pvTxData into the message buffer. When a message is written to the message buffer an additional sizeof( size_t ) bytes are also written to store the message's length. sizeof( size_t ) is typically 4 bytes on a 32-bit architecture, so on most 32-bit architecture setting xDataLengthBytes to 20 will reduce the free space in the message buffer by 24 bytes (20 bytes of message data and 4 bytes to hold the message length).
pxHigherPriorityTaskWokenIt is possible that a message buffer will have a task blocked on it waiting for data. Calling xMessageBufferSendFromISR() can make data available, and so cause a task that was waiting for data to leave the Blocked state. If calling xMessageBufferSendFromISR() causes a task to leave the Blocked state, and the unblocked task has a priority higher than the currently executing task (the task that was interrupted), then, internally, xMessageBufferSendFromISR() will set *pxHigherPriorityTaskWoken to pdTRUE. If xMessageBufferSendFromISR() sets this value to pdTRUE, then normally a context switch should be performed before the interrupt is exited. This will ensure that the interrupt returns directly to the highest priority Ready state task. *pxHigherPriorityTaskWoken should be set to pdFALSE before it is passed into the function. See the code example below for an example.
Returns
The number of bytes actually written to the message buffer. If the message buffer didn't have enough free space for the message to be stored then 0 is returned, otherwise xDataLengthBytes is returned.

Example use:

// A message buffer that has already been created.
MessageBufferHandle_t xMessageBuffer;
void vAnInterruptServiceRoutine( void )
{
size_t xBytesSent;
char *pcStringToSend = "String to send";
BaseType_t xHigherPriorityTaskWoken = pdFALSE; // Initialised to pdFALSE.

// Attempt to send the string to the message buffer.
xBytesSent = xMessageBufferSendFromISR( xMessageBuffer,
                                        ( void * ) pcStringToSend,
                                        strlen( pcStringToSend ),
                                        &xHigherPriorityTaskWoken );

if( xBytesSent != strlen( pcStringToSend ) )
{
    // The string could not be added to the message buffer because there was
    // not enough free space in the buffer.
}

// If xHigherPriorityTaskWoken was set to pdTRUE inside
// xMessageBufferSendFromISR() then a task that has a priority above the
// priority of the currently executing task was unblocked and a context
// switch should be performed to ensure the ISR returns to the unblocked
// task.  In most FreeRTOS ports this is done by simply passing
// xHigherPriorityTaskWoken into taskYIELD_FROM_ISR(), which will test the
// variables value, and perform the context switch if necessary.  Check the
// documentation for the port in use for port specific instructions.
taskYIELD_FROM_ISR( xHigherPriorityTaskWoken );

}