SDK provide eDMA transactional APIs to transfer data using eDMA, the eDMA method is similar with interrupt transactional method.  
More...
- Note
 - eDMA transactional functions use multiple beats method for better performance, in contrast, the blocking functions and interupt functions use single beat method. The function FLEXIO_MCULCD_ReadData, FLEXIO_MCULCD_WriteData, FLEXIO_MCULCD_GetStatusFlags, and FLEXIO_MCULCD_ClearStatusFlags are only used for single beat case, so don't use these functions to work together with eDMA functions.
 
flexio_MCULCD_edma_handle_t handle;
volatile bool completeFlag = false;
{
    {
        completeFlag = true;
    }
}
void main(void)
{
    
    
    
    
    
    
    
    FLEXIO_MCULCD_TransferCreateHandleEDMA(&flexioLcdDev, &handle, flexioLcdCallback, NULL, &txEdmaHandle, &rxEdmaHandle);
    xfer.command = command2;
    xfer.dataAddrOrSameValue = (uint32_t)dataToSend;
    xfer.dataCount = sizeof(dataToSend);
    completeFlag = false;
    FLEXIO_MCULCD_TransferEDMA(&flexioLcdDev, &handle, &xfer);
    while (!completeFlag)
    {
    }
    xfer.command = command2;
    xfer.dataAddrOrSameValue = value;
    xfer.dataCount = 1000;
    completeFlag = false;
    FLEXIO_MCULCD_TransferEDMA(&flexioLcdDev, &handle, &xfer);
    while (!completeFlag)
    {
    }
    xfer.command = command3;
    xfer.dataAddrOrSameValue = (uint32_t)dataToReceive;
    xfer.dataCount = sizeof(dataToReceive);
    completeFlag = false;
    FLEXIO_MCULCD_TransferEDMA(&flexioLcdDev, &handle, &xfer);
    while (!completeFlag)
    {
    }
}