Fixes:
- Fix a memory leak when realloc fails (see #267), thanks for reporting
- Fix a typo in the header file (see #266), thanks
1.7.6
Fixes:
- Add
SONAME to the ELF files built by the Makefile (see #252), thanks for reporting
- Add include guards and
extern "C" to cJSON_Utils.h (see #256), thanks for reporting
Other changes:
- Mark the Makefile as deprecated in the README.
1.7.5
Fixes:
- Fix a bug in the JSON Patch implementation of
cJSON Utils (see #251), thanks .
1.7.4
Fixes:
- Fix potential use after free if the
string parameter to cJSON_AddItemToObject is an alias of the string property of the object that is added (#248). Thanks for reporting.
1.7.3
Fixes:
- Fix potential double free, thanks for reporting (see #241)
1.7.2
Fixes:
- Fix the use of GNUInstallDirs variables and the pkgconfig file. Thanks for reporting (see #240)
1.7.1
Fixes:
- Fixed an Off-By-One error that could lead to an out of bounds write. Thanks for reporting (see #230)
- Fixed two errors with buffered printing. Thanks for reporting (see #230)
1.7.0
Features:
- Large rewrite of the documentation, see #215
- Added the
cJSON_GetStringValue function
- Added the
cJSON_CreateStringReference function
- Added the
cJSON_CreateArrayReference function
- Added the
cJSON_CreateObjectReference function
- The
cJSON_Add...ToObject macros are now functions that return a pointer to the added item, see #226
Fixes:
- Fix a problem with
GNUInstallDirs in the CMakeLists.txt, thanks , see #210
- Fix linking the tests when building as static library, see #213
- New overrides for the CMake option
BUILD_SHARED_LIBS, see #207
Other Changes:
- Readme: Explain how to include cJSON, see #211
- Removed some trailing spaces in the code, thanks , see#212
- Updated Unity and json-patch-tests
1.6.0
Features:
- You can now build cJSON as both shared and static library at once with CMake using
-DBUILD_SHARED_AND_STATIC_LIBS=On, see #178
- UTF-8 byte order marks are now ignored, see #184
- Locales can now be disabled with the option
-DENABLE_LOCALES=Off, see #202, thanks
- Better support for MSVC and Visual Studio
Other Changes:
- Add the new warnings
-Wswitch-enum, -Wused-but-makred-unused, -Wmissing-variable-declarations, -Wunused-macro
- More number printing tests.
- Continuous integration testing with AppVeyor (semi automatic at this point), thanks -p-r
1.5.9
- Set the global error pointer even if
return_parse_end is passed to cJSON_ParseWithOpts. See #200, thanks
1.5.8
- Fix
make test in the Makefile, thanks for reporting this (#195)
1.5.7
Fixes:
- Fix a bug where realloc failing would return a pointer to an invalid memory address. This is a security issue as it could potentially be used by an attacker to write to arbitrary memory addresses. (see #189), fixed in (954d61e5e7cb9dc6c480fc28ac1cdceca07dd5bd), big thanks for reporting this issue
- Fix a spelling mistake in the AFL fuzzer dictionary (#185), thanks
1.5.6
Fixes:
- Make cJSON a lot more tolerant about passing NULL pointers to its functions, it should now fail safely instead of dereferencing the pointer. (#183) Thanks for reporting #182
1.5.5
Fixes:
- Fix pointers to nested arrays in cJSON_Utils (9abe75e072050f34732a7169740989a082b65134)
- Fix an error with case sensitivity handling in cJSON_Utils (b9cc911831b0b3e1bb72f142389428e59f882b38)
- Fix cJSON_Compare for arrays that are prefixes of the other and objects that are a subset of the other (03ba72faec115160d1f3aea5582d9b6af5d3e473) See #180, thanks for reporting
1.5.4
Fixes:
- Fix build with GCC 7.1.1 and optimization level
-O2 (bfbd8fe0d85f1dd21e508748fc10fc4c27cc51be)
Other Changes:
- Update Unity to 3b69beaa58efc41bbbef70a32a46893cae02719d
1.5.3
Fixes:
- Fix
cJSON_ReplaceItemInObject not keeping the name of an item (#174)
1.5.2
Fixes:
- Fix a reading buffer overflow in
parse_string (a167d9e381e5c84bc03de4e261757b031c0c690d)
- Fix compiling with -Wcomma (186cce3ece6ce6dfcb58ac8b2a63f7846c3493ad)
- Remove leftover attribute from tests (b537ca70a35680db66f1f5b8b437f7114daa699a)
1.5.1
Fixes:
- Add gcc version guard to the Makefile (#164), thanks
- Fix incorrect free in
cJSON_Utils if custom memory allocator is used (#166), thanks
1.5.0
Features:
- cJSON finally prints numbers without losing precision (#153) thanks
cJSON_Compare recursively checks if two cJSON items contain the same values (#148)
- Provide case sensitive versions of every function where it matters (#158, #159)
- Added
cJSON_ReplaceItemViaPointer and cJSON_DetachItemViaPointer
- Added
cJSON_free and cJSON_malloc that expose the internal configured memory allocators. (02a05eea4e6ba41811f130b322660bea8918e1a0)
Enhancements:
- Parse into a buffer, this will allow parsing
\u0000 in the future (not quite yet though)
- General simplifications and readability improvements
- More unit tests
- Update unity testing library to 2.4.1
- Add the json-patch-tests test suite to test cJSON_Utils.
- Move all tests from
test_utils.c to unit tests with unity.
Fixes:
- Fix some warnings with the Microsoft compiler (#139) thanks
- Fix several bugs in cJSON_Utils, mostly found with json-patch-tests
- Prevent a stack overflow by specifying a maximum nesting depth
CJSON_NESTING_LIMIT
Other Changes:
- Move generated files in the
library_config subdirectory.
1.4.7
Fixes:
- Fix
cJSONUtils_ApplyPatches, it was completely broken and apparently nobody noticed (or at least reported it) (075a06f40bdc4f836c7dd7cad690d253a57cfc50)
- Fix inconsistent prototype for
cJSON_GetObjectItemCaseSensitive (51d3df6c9f7b56b860c8fb24abe7bab255cd4fa9) thanks
1.4.6
Fixes:
- Several corrections in the README
- Making clear that
valueint should not be written to
- Fix overflow detection in
ensure (2683d4d9873df87c4bdccc523903ddd78d1ad250)
- Fix a potential null pointer dereference in cJSON_Utils (795c3acabed25c9672006b2c0f40be8845064827)
- Replace incorrect `sizeof('\0')
withsizeof("")` (84237ff48e69825c94261c624eb0376d0c328139)
- Add caveats section to the README (50b3c30dfa89830f8f477ce33713500740ac3b79)
- Make cJSON locale independent (#146) Thanks for reporting
- Fix compiling without CMake with MSVC (#147) Thanks for reporting
1.4.5
Fixes:
- Fix bug in
cJSON_SetNumberHelper, thanks (#138 ef34500693e8c4a2849d41a4bd66fd19c9ec46c2)
- Workaround for internal compiler error in GCC 5.4.0 and 6.3.1 on x86 (2f65e80a3471d053fdc3f8aed23d01dd1782a5cb GCC bugreport)
1.4.4
Fixes:
- Fix a theoretical integer overflow, (not sure if it is possible on actual hardware) e58f7ec027d00b7cdcbf63e518c1b5268b29b3da
- Fix an off by one error (cc84a446be20cc283bafdc4d94c050ba1111ac02), thanks
- Double check the offset of the print buffer in
ensure (1934059554b9a0971e00f79e96900f422cfdd114)
Improvements:
- Add a note in the header about required buffer size when using
cJSON_PrintPreallocated (4bfb88009342fb568295a7f6dc4b7fee74fbf022)
1.4.3
Fixes:
- Fix compilation of the tests on 32 bit PowerPC and potentially other systems (4ec6e76ea2eec16f54b58e8c95b4c734e59481e4)
- Fix compilation with old GCC compilers (4.3+ were tested) (227d3398d6b967879761ebe02c1b63dbd6ea6e0d, 466eb8e3f8a65080f2b3ca4a79ab7b72bd539dba), see also #126
1.4.2
Fixes:
- Fix minimum required cmake version (30e1e7af7c63db9b55f5a3cda977a6c032f0b132)
- Fix detection of supported compiler flags (76e5296d0d05ceb3018a9901639e0e171b44a557)
- Run
cJSON_test and cJSON_test_utils along with unity tests (c597601cf151a757dcf800548f18034d4ddfe2cb)
1.4.1
Fix: Make print_number abort with a failure in out of memory situations (cf1842dc6f64c49451a022308b4415e4d468be0a)
1.4.0
Features
- Functions to check the type of an item (#120)
- Use dllexport on windows and fvisibility on Unix systems for public functions (#116), thanks
- Remove trailing zeroes from printed numbers (#123)
- Expose the internal boolean type
cJSON_bool in the header (2d3520e0b9d0eb870e8886e8a21c571eeddbb310)
Fixes
- Fix handling of NULL pointers in
cJSON_ArrayForEach (b47d0e34caaef298edfb7bd09a72cfff21d231ff)
- Make it compile with GCC 7 (fix -Wimplicit-fallthrough warning) (9d07917feb1b613544a7513d19233d4c851ad7ad)
Other Improvements
- internally use realloc if available (#110)
- builtin support for fuzzing with afl (#111)
- unit tests for the print functions (#112)
- Always use buffered printing (#113)
- simplify the print functions (#114)
- Add the compiler flags
-Wdouble-conversion, -Wparentheses and -Wcomma (#122)
1.3.2
Fix:
- Don't build the unity library if testing is disabled ( #121 ). Thanks
1.3.1
Bugfix release that fixes an out of bounds read #118. This shouldn't have any security implications.
1.3.0
This release includes a lot of rework in the parser and includes the Cunity unit testing framework, as well as some fixes. I increased the minor version number because there were quite a lot of internal changes.
Features:
- New type for cJSON structs:
cJSON_Invalid (#108)
Fixes:
- runtime checks for a lot of potential integer overflows
- fix incorrect return in cJSON_PrintBuffered (cf9d57d56cac21fc59465b8d26cf29bf6d2a87b3)
- fix several potential issues found by Coverity
- fix potentially undefined behavior when assigning big numbers to
valueint (41e2837df1b1091643aff073f2313f6ff3cc10f4)
- Numbers exceeding
INT_MAX or lower than INT_MIN will be explicitly assigned to valueint as INT_MAX and INT_MIN respectively (saturation on overflow).
- fix the
cJSON_SetNumberValue macro (87f77274de6b3af00fb9b9a7f3b900ef382296c2), this slightly changes the behavior, see commit message
Introduce unit tests
Started writing unit tests with the Cunity testing framework. Currently this covers the parser functions.
Also:
Simplifications
After having unit tests for the parser function in place, I started refactoring the parser functions (as well as others) and making them easier to read and maintain.
- Use
strtod from the standard library for parsing numbers (074766997246481dfc72bfa78f07898a2716473f)
- Use goto-fail in several parser functions (#100)
- Rewrite/restructure all of the parsing functions to be easier to understand and have less code paths doing the same as another. (#109)
- Simplify the buffer allocation strategy to always doubling the needed amount (9f6fa94c91a87b71e4c6868dbf2ce431a48517b0)
- Combined
cJSON_AddItemToObject and cJSON_AddItemToObjectCS to one function (cf862d0fed7f9407e4b046d78d3d8050d2080d12)
Other changes
- Prevent the usage of incompatible C and header versions via preprocessor directive (123bb1af7bfae41d805337fef4b41045ef6c7d25)
- Let CMake automatically detect compiler flags
- Add new compiler flags (
-Wundef, -Wswitch-default, -Wconversion, -fstack-protector-strong) (#98)
- Change internal sizes from
int to size_t (ecd5678527a6bc422da694e5be9e9979878fe6a0)
- Change internal strings from
char* to unsigned char* (28b9ba4334e0f7309e867e874a31f395c0ac2474)
- Add
const in more places
1.2.1
Fixes:
- Fixes a potential null pointer dereference in cJSON_Utils, discovered using clang's static analyzer by -nf (#96)
1.2.0
Features:
- Add a new type of cJSON item for raw JSON and support printing it. Thanks (#65, #90)
Fixes:
- Compiler warning if const is casted away, Thanks (#83)
- Fix compile error with strict-overflow on PowerPC, (#85)
- Fix typo in the README, thanks (#88)
- Add compile flag for compatibility with C++ compilers
1.1.0
- Add a function
cJSON_PrintPreallocated to print to a preallocated buffer, thanks (#72)
- More compiler warnings when using Clang or GCC, thanks (#75, #78)
- fixed a memory leak in
cJSON_Duplicate, thanks (#81)
- fix the
ENABLE_CUSTOM_COMPILER_FLAGS cmake option
1.0.2
Rename internal boolean type, see #71.
1.0.1
Small bugfix release.
- Fixes a bug with the use of the cJSON structs type in cJSON_Utils, see d47339e2740360e6e0994527d5e4752007480f3a
- improve code readability
- initialize all variables
1.0.0
This is the first official versioned release of cJSON. It provides an API version for the shared library and improved Makefile and CMake build files.