![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
A little fail-safe filesystem designed for embedded systems.
``` | | | .—._____ .--—. | | –|o |—| littlefs | –| |—| | '--—' '-------—' | | | ```
Bounded RAM/ROM - The littlefs is designed to work with a limited amount of memory. Recursion is avoided and dynamic memory is limited to configurable buffers that can be provided statically.
Power-loss resilient - The littlefs is designed for systems that may have random power failures. The littlefs has strong copy-on-write guarantees and storage on disk is always kept in a valid state.
Wear leveling - Since the most common form of embedded storage is erodible flash memories, littlefs provides a form of dynamic wear leveling for systems that can not fit a full flash translation layer.
Here's a simple example that updates a file named boot_count every time main runs. The program can be interrupted at any time without losing track of how many times it has been booted and without corrupting the filesystem:
``` c #include "lfs.h"
// variables used by the filesystem lfs_t lfs; lfs_file_t file;
// configuration of the filesystem is provided by this struct const struct lfs_config cfg = { // block device operations .read = user_provided_block_device_read, .prog = user_provided_block_device_prog, .erase = user_provided_block_device_erase, .sync = user_provided_block_device_sync,
// block device configuration .read_size = 16, .prog_size = 16, .block_size = 4096, .block_count = 128, .lookahead = 128, };
// entry point int main(void) { // mount the filesystem int err = lfs_mount(&lfs, &cfg);
// reformat if we can't mount the filesystem // this should only happen on the first boot if (err) { lfs_format(&lfs, &cfg); lfs_mount(&lfs, &cfg); }
// read current count uint32_t boot_count = 0; lfs_file_open(&lfs, &file, "boot_count", LFS_O_RDWR | LFS_O_CREAT); lfs_file_read(&lfs, &file, &boot_count, sizeof(boot_count));
// update boot count boot_count += 1; lfs_file_rewind(&lfs, &file); lfs_file_write(&lfs, &file, &boot_count, sizeof(boot_count));
// remember the storage is not updated until the file is closed successfully lfs_file_close(&lfs, &file);
// release any resources we were using lfs_unmount(&lfs);
// print the boot count printf("boot_count: %d\n", boot_count); } ```
Detailed documentation (or at least as much detail as is currently available) can be found in the comments in lfs.h.
As you may have noticed, littlefs takes in a configuration structure that defines how the filesystem operates. The configuration struct provides the filesystem with the block device operations and dimensions, tweakable parameters that tradeoff memory usage for performance, and optional static buffers if the user wants to avoid dynamic memory.
The state of the littlefs is stored in the lfs_t type which is left up to the user to allocate, allowing multiple filesystems to be in use simultaneously. With the lfs_t and configuration struct, a user can format a block device or mount the filesystem.
Once mounted, the littlefs provides a full set of POSIX-like file and directory functions, with the deviation that the allocation of filesystem structures must be provided by the user.
All POSIX operations, such as remove and rename, are atomic, even in event of power-loss. Additionally, no file updates are actually committed to the filesystem until sync or close is called on the file.
All littlefs have the potential to return a negative error code. The errors can be either one of those found in the enum lfs_error in lfs.h, or an error returned by the user's block device operations.
It should also be noted that the current implementation of littlefs doesn't really do anything to ensure that the data written to disk is machine portable. This is fine as long as all of the involved machines share endianness (little-endian) and don't have strange padding requirements.
DESIGN.md - DESIGN.md contains a fully detailed dive into how littlefs actually works. I would encourage you to read it since the solutions and tradeoffs at work here are quite interesting.
SPEC.md - SPEC.md contains the on-disk specification of littlefs with all the nitty-gritty details. Can be useful for developing tooling.
The littlefs comes with a test suite designed to run on a PC using the emulated block device found in the emubd directory. The tests assume a Linux environment and can be started with make:
``` bash make test ```
Mbed OS - The easiest way to get started with littlefs is to jump into Mbed, which already has block device drivers for most forms of embedded storage. The littlefs is available in Mbed OS as the LittleFileSystem class.
littlefs-fuse - A FUSE wrapper for littlefs. The project allows you to mount littlefs directly on a Linux machine. Can be useful for debugging littlefs if you have an SD card handy.
littlefs-js - A javascript wrapper for littlefs. I'm not sure why you would want this, but it is handy for demos. You can see it in action here.