![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
A truly complete and generic sequence for initializing the lwIP stack cannot be given because it depends on additional initializations for your runtime environment (e.g. timers).
We can give you some idea on how to proceed when using the raw API. We assume a configuration using a single Ethernet netif and the UDP and TCP transport layers, IPv4 and the DHCP client.
Call these functions in the order of appearance:
netif_add(struct netif *netif, ...): Adds your network interface to the netif_list. Allocate a struct netif and pass a pointer to this structure as the first argument. Give pointers to cleared ip_addr structures when using DHCP, or fill them with sane numbers otherwise. The state pointer may be NULL.
The init function pointer must point to a initialization function for your Ethernet netif interface. The following code illustrates its use.
For Ethernet drivers, the input function pointer must point to the lwIP function ethernet_input() declared in "netif/etharp.h". Other drivers must use ip_input() declared in "lwip/ip.h".