![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The Message Digest (MD) or Hashing module provides one-way hashing functions. Such functions can be used for creating a hash message authentication code (HMAC) when sending a message. Such a HMAC can be used in combination with a private key for authentication, which is a message integrity control.
All hash algorithms can be accessed via the generic MD layer (see mbedtls_md_setup())
The following hashing-algorithms are provided:
This module provides one-way hashing which can be used for authentication.