MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

This section describes the programming interface of the UART Cortex Microcontroller Software Interface Standard (CMSIS) driver. And this driver defines generic peripheral driver interfaces for middleware making it reusable across a wide range of supported microcontroller devices. The API connects microcontroller peripherals with middleware that implements for example communication stacks, file systems, or graphic user interfaces. More information and usage methord see http://www.keil.com/pack/doc/cmsis/Driver/html/index.html.

The UART driver includes transactional APIs.

Transactional APIs can be used to enable the peripheral quickly and in the application if the code size and performance of transactional APIs can satisfy the requirements. If the code size and performance are critical requirements please write custom code.

UART CMSIS Driver

UART Send/receive using an interrupt method

/* UART callback */
void UART_Callback(uint32_t event)
{
if (event == ARM_USART_EVENT_SEND_COMPLETE)
{
txBufferFull = false;
txOnGoing = false;
}
if (event == ARM_USART_EVENT_RECEIVE_COMPLETE)
{
rxBufferEmpty = false;
rxOnGoing = false;
}
}
Driver_USART0.Initialize(UART_Callback);
Driver_USART0.PowerControl(ARM_POWER_FULL);
/* Send g_tipString out. */
txOnGoing = true;
Driver_USART0.Send(g_tipString, sizeof(g_tipString) - 1);
/* Wait send finished */
while (txOnGoing)
{
}

UART Send/Receive using the DMA method

/* UART callback */
void UART_Callback(uint32_t event)
{
if (event == ARM_USART_EVENT_SEND_COMPLETE)
{
txBufferFull = false;
txOnGoing = false;
}
if (event == ARM_USART_EVENT_RECEIVE_COMPLETE)
{
rxBufferEmpty = false;
rxOnGoing = false;
}
}
Driver_USART0.Initialize(UART_Callback);
DMAMGR_Init();
Driver_USART0.PowerControl(ARM_POWER_FULL);
/* Send g_tipString out. */
txOnGoing = true;
Driver_USART0.Send(g_tipString, sizeof(g_tipString) - 1);
/* Wait send finished */
while (txOnGoing)
{
}