MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
Main Page
Related Pages
API Reference
All
Data Structures
Functions
Variables
Typedefs
Enumerations
Enumerator
Groups
Pages
Deprecated List
Global
CLOCK_SetUARTFRGMULT
(uint32_t mul)
Do not use this function. Refer to CLOCK_SetFRGClkMul().
Global
SCTIMER_SetupNextStateAction
(SCT_Type *base, uint32_t nextState, uint32_t event)
Do not use this function. It has been superceded by
SCTIMER_SetupNextStateActionwithLdMethod
Global
WWDT_Disable
(WWDT_Type *base)
Do not use this function. It will be deleted in next release version, for once the bit field of WDEN written with a 1, it can not be re-written with a 0.
© 2016 NXP Semiconductors. All rights reserved.