![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The flash provides the C90TFS Flash driver of Kinetis devices with the C90TFS Flash module inside. The flash driver provides general APIs to handle specific operations on C90TFS/FTFx Flash module. The user can use those APIs directly in the application. In addition, it provides internal functions called by the driver. Although these functions are not meant to be called from the user's application directly, the APIs can still be used.
Modules | |
Ftftx CACHE Driver | |
Ftftx FLASH Driver | |
Ftftx FLEXNVM Driver | |
ftfx controller | |
ftfx feature | |