![]() |
Kinetis SDK v.2.0 API Reference Manual
Rev. 0
NXP Semiconductors
|
SPI driver includes functional APIs and transactional APIs.
Functional APIs are feature/property target low level APIs. Functional APIs can be used for SPI initialization/configuration/operation for optimization/customization purpose. Using the functional API requires the knowledge of the SPI peripheral and how to organize functional APIs to meet the application requirements. All functional API use the peripheral base address as the first parameter. SPI functional operation groups provide the functional API set.
Transactional APIs are transaction target high level APIs. Transactional APIs can be used to enable the peripheral and in the application if the code size and performance of transactional APIs satisfy the requirements. If the code size and performance are a critical requirement, see the transactional API implementation and write a custom code. All transactional APIs use the spi_handle_t as the first parameter. Initialize the handle by calling the SPI_MasterTransferCreateHandle() or SPI_SlaveTransferCreateHandle() API.
Transactional APIs support asynchronous transfer. This means that the functions SPI_MasterTransferNonBlocking() and SPI_SlaveTransferNonBlocking() set up the interrupt for data transfer. When the transfer completes, the upper layer is notified through a callback function with the kStatus_SPI_Idle status.
Modules | |
| SPI DMA Driver | |
| SPI Driver | |
| SPI FreeRTOS driver | |