MCUXpresso SDK API Reference Manual  Rev 2.11.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Smart Card UART Driver

The Smart Card UART driver uses a standard UART peripheral which supports the ISO-7816 standard. The driver supports transmission functionality in the CPU mode. The driver also supports non-blocking (asynchronous) type of data transfers. The blocking (synchronous) transfer is supported only by the RTOS adaptation layer.