![]() |
MCUXpresso SDK API Reference Manual
Rev 2.13.0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Digital Microphone (DMIC) module.
The DMIC driver is created to help the user more easily operate the DMIC module. This driver can be used to performed basic and advanced DMIC operations. The driver can be used to transfer data from DMIC to memory using DMA as well as in interrupt mode. The DMIC and DMA transfer in pingpong mode is preferred as DMIC is a streaming device.
This function group implements DMIC initialization and deinitialization API. DMIC_Init() function Enables the clock to the DMIC register interface. DMIC_Dinit() function Disables the clock to the DMIC register interface.
This function group implements DMIC configration API. DMIC_ConfigIO()function configures the use of PDM (Pulse Density moulation) pins. DMIC_SetOperationMode()function configures the mode of operation either in DMA or in interrupt. DMIC_ConfigChannel() function configures the various property of a DMIC channel. DMIC_Use2fs()function configures the clock scaling used for PCM data output. DMIC_EnableChannnel() function enables a particualr DMIC channel. DMIC_FifoChannel() function configures FIFO settings for a DMIC channel.
This function group implements the API to get data and status of DMIC FIFO. DMIC_FifoGetStatus() function gives the status of a DMIC FIFO. DMIC_ClearStatus() function clears the status of a DMIC FIFO. DMIC_FifoGetData() function gets data from a DMIC FIFO.
DMIC_EnablebleIntCallback() enables the interrupt for the selected DMIC peripheral. DMIC_DisableIntCallback() disables the interrupt for the selected DMIC peripheral.
This function group implements the API for HWVAD. DMIC_SetGainNoiseEstHwvad() Sets the gain value for the noise estimator. DMIC_SetGainSignalEstHwvad() Sets the gain value for the signal estimator. DMIC_SetFilterCtrlHwvad() Sets the HWVAD filter cutoff frequency parameter. DMIC_SetInputGainHwvad() Sets the input gain of HWVAD. DMIC_CtrlClrIntrHwvad() Clears HWVAD internal interrupt flag. DMIC_FilterResetHwvad() Resets HWVAD filters. DMIC_GetNoiseEnvlpEst() Gets the value from output of the filter z7.
DMIC_HwvadEnableIntCallback() enables the HWVAD interrupt for the selected DMIC peripheral. DMIC_HwvadDisableIntCallback() disables the HWVAD interrupt for the selected DMIC peripheral.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/dmic
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/dmic
Modules | |
| DMIC DMA Driver | |
| DMIC Driver | |