![]() |
MCUXpresso SDK API Reference Manual
Rev 2.13.1
NXP Semiconductors
|
The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' src operation.
The Power Gating and Memory Controller(PGMC) block is a power management component that controls power gating of power domains and memory low power mode. There are four sub modules in the PGMC block, they are:
For the BPC sub module, the APIs in "Basic Power Controller Related Interfaces" function group are provided. For the CPC sub module, the APIs in "CPU Power Controller Related Interfaces" function group are provided. For the PPC sub module, the APIs in "PMIC Power Related Interfaces" function group are provided. For the MIF sub module, the APIs in "MIF Module Related APIs" are provided.