![]() |
MCUXpresso SDK API Reference Manual
Rev 2.14.0
NXP Semiconductors
|
This section describes the programming interface of the FGPIO driver. The FGPIO driver configures the FGPIO module and provides a functional interface to build the GPIO application.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/gpio
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/gpio
This section describes the programming interface of the FGPIO driver. The FGPIO driver configures the FGPIO module and provides a functional interface to build the RGPIO application.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/rgpio
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/rgpio