MCUXpresso SDK API Reference Manual  Rev 2.14.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
ENET CMSIS Driver

This section describes the programming interface of the ENET Cortex Microcontroller Software Interface Standard (CMSIS) driver. This driver defines generic peripheral driver interfaces for middleware making it reusable across a wide range of supported microcontroller devices. The API connects microcontroller peripherals with middleware that implements for example communication stacks, file systems, or graphic user interfaces. More information and usage methord see http://www.keil.com/pack/doc/cmsis/Driver/html/index.html.

The ENET CMSIS driver includes transactional APIs.

Transactional APIs are transaction target high-level APIs. The transactional APIs can be used to enable the peripheral quickly and also in the application if the code size and performance of transactional APIs satisfy the requirements. If the code size and performance are critical requirements, see the transactional API implementation and write custom code accessing the hardware registers.

Typical use case

void ENET_SignalEvent_t(uint32_t event)
{
if (event == ARM_ETH_MAC_EVENT_RX_FRAME)
{
uint32_t size;
uint32_t len;
/* Get the Frame size */
size = EXAMPLE_ENET.GetRxFrameSize();
/* Call ENET_ReadFrame when there is a received frame. */
if (size != 0)
{
/* Received valid frame. Deliver the rx buffer with the size equal to length. */
uint8_t *data = (uint8_t *)malloc(size);
if (data)
{
len = EXAMPLE_ENET.ReadFrame(data, size);
if (size == len)
{
/* Increase the received frame numbers. */
if (g_rxIndex < ENET_EXAMPLE_LOOP_COUNT)
{
g_rxIndex++;
}
}
free(data);
}
}
}
if (event == ARM_ETH_MAC_EVENT_TX_FRAME)
{
g_testTxNum ++;
}
}
/* Initialize the ENET module. */
EXAMPLE_ENET.Initialize(ENET_SignalEvent_t);
EXAMPLE_ENET.PowerControl(ARM_POWER_FULL);
EXAMPLE_ENET.SetMacAddress((ARM_ETH_MAC_ADDR *)g_macAddr);
EXAMPLE_ENET.Control(ARM_ETH_MAC_CONFIGURE, linkInfo.speed << ARM_ETH_MAC_SPEED_Pos |
linkInfo.duplex << ARM_ETH_MAC_DUPLEX_Pos | ARM_ETH_MAC_ADDRESS_BROADCAST);
EXAMPLE_ENET_PHY.PowerControl(ARM_POWER_FULL);
EXAMPLE_ENET_PHY.SetMode(ARM_ETH_PHY_AUTO_NEGOTIATE);
EXAMPLE_ENET.Control(ARM_ETH_MAC_CONTROL_RX, 1);
EXAMPLE_ENET.Control(ARM_ETH_MAC_CONTROL_TX, 1);
if (EXAMPLE_ENET_PHY.GetLinkState() == ARM_ETH_LINK_UP)
{
linkInfo = EXAMPLE_ENET_PHY.GetLinkInfo();
}
else
{
PRINTF("\r\nPHY Link down, please check the cable connection and link partner setting.\r\n");
}
/* Build broadcast for sending. */
ENET_BuildBroadCastFrame();
while (1)
{
/* Check the total number of received number. */
if (g_rxCheckIdx != g_rxIndex)
{
PRINTF("The %d frame has been successfuly received!\r\n", g_rxIndex);
g_rxCheckIdx = g_rxIndex;
}
if ( g_testTxNum && (g_txCheckIdx != g_testTxNum))
{
g_txCheckIdx = g_testTxNum;
PRINTF("The %d frame transmitted success!\r\n", g_txCheckIdx);
}
/* Get the Frame size */
if (txnumber < ENET_EXAMPLE_LOOP_COUNT)
{
txnumber ++;
/* Send a multicast frame when the PHY is link up. */
if (EXAMPLE_ENET.SendFrame(&g_frame[0], ENET_DATA_LENGTH, ARM_ETH_MAC_TX_FRAME_EVENT) == ARM_DRIVER_OK)
{
for (uint32_t count = 0; count < 0x3FF; count++)
{
__ASM("nop");
}
}
else
{
PRINTF(" \r\nTransmit frame failed!\r\n");
}
}
}