MCUXpresso SDK API Reference Manual  Rev 2.15.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Deprecated List
Global CS42888_SetFuncMode (cs42888_handle_t *handle, cs42888_func_mode mode)
api, Do not use it anymore. It has been superceded by CS42888_SelectFunctionalMode.
Global DCDC_AdjustTargetVoltage (DCDC_Type *base, uint32_t VDDRun, uint32_t VDDStandby)
Do not use this function. It has been superceded by DCDC_AdjustRunTargetVoltage and DCDC_AdjustLowPowerTargetVoltage
Global GPIO_ClearPinsOutput (GPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by GPIO_PortClear.
Global GPIO_DisableInterrupts (GPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by GPIO_PortDisableInterrupts.
Global GPIO_ReadPadStatus (GPIO_Type *base, uint32_t pin)
Do not use this function. It has been superceded by GPIO_PinReadPadStatus.
Global GPIO_ReadPinInput (GPIO_Type *base, uint32_t pin)
Do not use this function. It has been superceded by GPIO_PinRead.
Global GPIO_SetPinInterruptConfig (GPIO_Type *base, uint32_t pin, gpio_interrupt_mode_t pinInterruptMode)
Do not use this function. It has been superceded by GPIO_PinSetInterruptConfig.
Global GPIO_SetPinsOutput (GPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by GPIO_PortSet.
Global GPIO_WritePinOutput (GPIO_Type *base, uint32_t pin, uint8_t output)
Do not use this function. It has been superceded by GPIO_PinWrite.
Global OCOTP_ReadFuseShadowRegister (OCOTP_Type *base, uint32_t address)
Use OCOTP_ReadFuseShadowRegisterExt instead of this function.
Global PMU_2P1EnablePullDown (PMU_Type *base, bool enable)
Do not use this function. It has been superceded by PMU_2P5EnablePullDown.
Global WM8904_SetMasterSlave (wm8904_handle_t *handle, bool master)
DO NOT USE THIS API ANYMORE. IT HAS BEEN SUPERCEDED BY WM8904_SetMasterClock