![]() |
MCUXpresso SDK API Reference Manual
Rev 2.14.0
NXP Semiconductors
|
Content including 1) peripheral features, work logic and work method; 2) driver design logic and use method; 3) typical use case. More...
This driver provides interfaces to initialize the EWM peripheral, then user can enable/disable interrupt on demand. For watch dog, there's a refresh function to reload it.
EWM is used to monitor the flow and execution of embedded software within an MCU, refresh operation should be periodically done, if the EWM is not refreshed in specified time window, EWM_Out signal will be asserted to to reset or place the external circuit into safe mode.