![]() |
MCUXpresso SDK API Reference Manual
Rev 2.15.100
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the 10/100/1000 Mbps Ethernet QoS with TSN module of MCUXpresso SDK devices.
Use the ENET_QOS_GetDefaultConfig() to get the default basic configuration, Use the default configuration unchanged or changed as the input to the ENET_QOS_Init() to do basic configuration for EQOS module. Call ENET_QOS_DescriptorInit() to initialization the descriptors and Call ENET_QOS_StartRxTx() to start the EQOS engine after all initialization. ENET_QOS_Deinit() is used to to EQOS De-initialization.
This group provides the EQOS mac address set/get operation with ENET_QOS_SetMacAddr() and ENET_QOS_GetMacAddr(). The ENET_QOS_EnterPowerDown() and ENET_QOS_ExitPowerDown() can be used to do power management.
This group provide the DMA interrupt get and clear APIs. This can be used by application to create new IRQ handler.
This group functions are low level TX/RX descriptor operations. It is convenient to use these TX/RX APIs to do application specific RX/TX. For TX: Use ENET_QOS_IsTxDescriptorDmaOwn(), ENET_QOS_SetupTxDescriptor() to build your packet for transfer and ENET_QOS_UpdateTxDescriptorTail to update the TX tail pointer. For RX: Use ENET_QOS_GetRxDescriptor() to get the received data/length and use the ENET_QOS_UpdateRxDescriptor() to update the buffers/status.
When use the Transactional APIs, please make sure to call the ENET_QOS_CreateHandler to create the handler which are used to maintain all data related to TX/RX process.
For EQOS receive, the ENET_QOS_GetRxFrameSize() function must be called to get the received data size. Then, call the ENET_QOS_ReadFrame() function to get the received data.
For EQOS transmit, call the ENET_QOS_SendFrame() function to send the data out. To save memory and avoid the memory copy in the TX process. The ENET_QOS_SendFrame() here is a zero-copy API, so make sure the input data buffers are not re-queued or freed before the data are really sent out. To make sure the data buffers reclaim is rightly done. the transmit interrupt must be used. so For transactional APIs here we enabled the tx interrupt in ENET_QOS_CreateHandler(). That means the tx interrupt is automatically enabled in transactional APIs. is recommended to be called on the transmit interrupt handler.ENET_QOS_ReclaimTxDescriptor() is a transactional API to get the information from the finished transmit data buffers and reclaim the tx index. it is called by the transmit interrupt IRQ handler.
For use the transactional APIs, receive polling Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/enet_qos For the functional API, rx polling Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/enet_qos