The current FLEXCAN driver version is 2.1.1.  
More...
- 2.1.1
- Bug Fixes
- Fixed the violation of MISRA-2012 rule.
 
- Fixed CBT SEG2 potential overflow issue.
 
 
 
- 2.1.0
- Improvement
- Add bEnableTimingCalc member in flexcan_config_t structure to make users can choose to use their desired timing values or use auto calculate timing values to initialize FLEXCAN module.
 
- Update FLEXCAN_CalculateImprovedTimingValues/FLEXCAN_FDCalculateImprovedTimingValues APIs to improvement the bit timing calculate.
 
- Add FLEXCAN_CalculateImprovedTimingValuesWithCBT API.
 
- Move TDC config operations to FLEXCAN_SetFDTimingConfig API.
 
- Add FLEXCAN_SetBaudRate/FLEXCAN_SetFDBaudRate APIs to enable auto update CAN bit timing configuration base on baud rate parameter.
 
- Update FLEXCAN_WriteFDTxMb to make it can send both CAN FD frame and classic frame.
 
 
 
- 2.0.2
- Bug Fixes
- Fixed build error by adding macro isolation to all CAN FD codes.
 
 
 
- 2.0.1
 
- 2.0.0