MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Deprecated List
Global flexcan_clock_source_t

Do not use the kFLEXCAN_ClkSrcOs. It has been superceded kFLEXCAN_ClkSrc0

Do not use the kFLEXCAN_ClkSrcPeri. It has been superceded kFLEXCAN_ClkSrc1

Class flexcan_config_t

Do not use the baudRate. It has been superceded bitRate

Do not use the baudRateFD. It has been superceded bitRateFD

Global I3C_SlaveRequestIBIWithSingleData (I3C_Type *base, uint8_t data, size_t dataSize)
Do not use this function. It has been superseded by I3C_SlaveRequestIBIWithData.
Global MMC_HostReset (SDMMCHOST_CONFIG *host)
Do not use this function. It has been superceded by MMC_HostDoReset. This function resets the specific host.
Global PDM_SetSampleRate (PDM_Type *base, uint32_t enableChannelMask, pdm_df_quality_mode_t qualityMode, uint8_t osr, uint32_t clkDiv)
Do not use this function. It has been superceded by PDM_SetSampleRateConfig
Global RGPIO_ClearPinsOutput (RGPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by RGPIO_PortClear.
Global RGPIO_ReadPinInput (RGPIO_Type *base, uint32_t pin)
Do not use this function. It has been superceded by RGPIO_PinRead.
Global RGPIO_SetPinsOutput (RGPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by RGPIO_PortSet.
Global RGPIO_TogglePinsOutput (RGPIO_Type *base, uint32_t mask)
Do not use this function. It has been superceded by RGPIO_PortToggle.
Global RGPIO_WritePinOutput (RGPIO_Type *base, uint32_t pin, uint8_t output)
Do not use this function. It has been superceded by RGPIO_PinWrite.
Global SEMC_ConfigureSRAM (SEMC_Type *base, semc_sram_config_t *config, uint32_t clkSrc_Hz)
Do not use this function. It has been superceded by SEMC_ConfigureSRAMWithChipSelection.
Global USDHC_AdjustDelayForManualTuning (USDHC_Type *base, uint32_t delay)
Do not use this function. It has been superceded by USDHC_SetTuingDelay