MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Deprecated List
Global flexcan_clock_source_t

Do not use the kFLEXCAN_ClkSrcOs. It has been superceded kFLEXCAN_ClkSrc0

Do not use the kFLEXCAN_ClkSrcPeri. It has been superceded kFLEXCAN_ClkSrc1

Class flexcan_config_t

Do not use the baudRate. It has been superceded bitRate

Do not use the baudRateFD. It has been superceded bitRateFD

Global I3C_SlaveRequestIBIWithSingleData (I3C_Type *base, uint8_t data, size_t dataSize)
Do not use this function. It has been superseded by I3C_SlaveRequestIBIWithData.
Global kSPC_CoreLDO_UnderDriveVoltage
, to align with description of latest RM, please use kSPC_Core_LDO_RetentionVoltage as instead.
Global kSPC_LowVoltageNormalLevel
, please use kSPC_LowVoltageHighRange as instead.
Global kSPC_LowVoltageSafeLevel
, please use kSPC_LowVoltageLowRange as instead.
Global SPC_SetSystemVDDLowVoltageLevel (SPC_Type *base, spc_low_voltage_level_select_t level)
In latest RM, reserved for all devices, will removed in next release.
Global spc_system_voltage_detect_config_t::level
, reserved for all devices, will removed in next release.
Global WWDT_Disable (WWDT_Type *base)
Do not use this function. It will be deleted in next release version, for once the bit field of WDEN written with a 1, it can not be re-written with a 0.