![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.100
NXP Semiconductors
|
The MCUXpresso SDK provides a driver for the Analog Converter (ACOMP) module of MCUXpreeso SDK devices.
The ACOMP driver can be divided into 4 function groups.
The functions in this group can be used to control the ACOMP module. User can invoke ACOMP_GetDefaultConfig() function to configure the default setting, then invoking ACOMP_Init() to initialize the module. All ACOMP feature(except software reset comparators and clock divider) can be enabled by invoking ACOMP_Init() function.
There is only one function in this function groups, it is ACOMP_GetResult(). User can get the result of comparator by invoking this function.
The functions in this group can be used to enable/disable interrupts.
The ACOMP_GetStatusFlags() function in this group can return all status flags. The ACOMP_ClearStatusFlags() can be used to clear status flags, but please note that no all status flags can be cleared by software.