MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

This section describes the programming interface of the USART Cortex Microcontroller Software Interface Standard (CMSIS) driver. And this driver defines generic peripheral driver interfaces for middleware making it reusable across a wide range of supported microcontroller devices. The API connects microcontroller peripherals with middleware that implements for example communication stacks, file systems, or graphic user interfaces. More information and usage methord see http://www.keil.com/pack/doc/cmsis/Driver/html/index.html.

The USART driver includes transactional APIs.

Transactional APIs can be used to enable the peripheral quickly and in the application if the code size and performance of transactional APIs can satisfy the requirements. If the code size and performance are critical requirements please write custom code.

USART Send Methods

USART Send/receive using an interrupt method

/* USART callback */
void USART_Callback(uint32_t event)
{
if (event == ARM_USART_EVENT_SEND_COMPLETE)
{
txOnGoing = false;
}
}
Driver_USART0.Initialize(USART_Callback);
Driver_USART0.PowerControl(ARM_POWER_FULL);
/* Send g_tipString out. */
txOnGoing = true;
Driver_USART0.Send(g_tipString, sizeof(g_tipString) - 1);
/* Wait send finished */
while (txOnGoing)
{
}

USART Send/Receive using the DMA method

/* USART callback */
void USART_Callback(uint32_t event)
{
if (event == ARM_USART_EVENT_SEND_COMPLETE)
{
txOnGoing = false;
}
}
Driver_USART0.Initialize(USART_Callback);
DMA_Init(DMA0);
Driver_USART0.PowerControl(ARM_POWER_FULL);
/* Send g_tipString out. */
txOnGoing = true;
Driver_USART0.Send(g_tipString, sizeof(g_tipString) - 1);
/* Wait send finished */
while (txOnGoing)
{
}