![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
The MCUXpresso SDK provides the peripheral driver for the I2S function of FLEXCOMM module of MCUXpresso SDK devices.
 
The I2S module is used to transmit or receive digital audio data. Only transmit or receive is enabled at one time in one module. 
Driver currently supports one (primary) channel pair per one I2S enabled FLEXCOMM module only. 
I2S_TxInit() and I2S_RxInit() functions ungate the clock for the FLEXCOMM module, assign I2S function to FLEXCOMM module and configure audio data format and other I2S operational settings. I2S_TxInit() is used when I2S should transmit data, I2S_RxInit() when it should receive data.
I2S_TxGetDefaultConfig() and I2S_RxGetDefaultConfig() functions can be used to set the module configuration structure with default values for transmit and receive function, respectively.
I2S_Deinit() function resets the FLEXCOMM module.
I2S_TxTransferCreateHandle() function creates transactional handle for transmit in interrupt mode.
I2S_RxTransferCreateHandle() function creates transactional handle for receive in interrupt mode.
I2S_TxTransferCreateHandleDMA() function creates transactional handle for transmit in DMA mode.
I2S_RxTransferCreateHandleDMA() function creates transactional handle for receive in DMA mode.
I2S_TxTransferNonBlocking() function is used to add data buffer to transmit in interrupt mode. It also begins transmission if not transmitting yet.
I2S_RxTransferNonBlocking() function is used to add data buffer to receive data into in interrupt mode. It also begins reception if not receiving yet.
I2S_TxTransferSendDMA() function is used to add data buffer to transmit in DMA mode. It also begins transmission if not transmitting yet.
I2S_RxTransferReceiveDMA() function is used to add data buffer to receive data into in DMA mode. It also begins reception if not receiving yet.
The transfer of data will be stopped automatically when all data buffers queued using the above functions will be processed and no new data buffer is enqueued meanwhile. If the above functions are not called frequently enough, I2S stop followed by restart may keep occurring resulting in drops audio stream.
I2S_EnableInterrupts() function is used to enable interrupts in FIFO interrupt register. Regular use cases do not require this function to be called from application code.
I2S_DisableInterrupts() function is used to disable interrupts in FIFO interrupt register. Regular use cases do not require this function to be called from application code.
I2S_GetEnabledInterrupts() function returns interrupts enabled in FIFO interrupt register. Regular use cases do not require this function to be called from application code.
I2S_TxHandleIRQ() and I2S_RxHandleIRQ() functions are called from ISR which is invoked when actual FIFO level decreases to configured watermark value.
I2S_DMACallback() function is called from ISR which is invoked when DMA transfer (actual descriptor) finishes.
I2S_Enable() function enables I2S function in FLEXCOMM module. Regular use cases do not require this function to be called from application code.
I2S_Disable() function disables I2S function in FLEXCOMM module. Regular use cases do not require this function to be called from application code.
I2S_TransferGetErrorCount() function returns the number of FIFO underruns or overruns in interrupt mode.
I2S_TransferGetCount() function returns the number of bytes transferred in interrupt mode.
I2S_TxTransferAbort() function aborts trasmit operation in interrupt mode.
I2S_RxTransferAbort() function aborts receive operation in interrupt mode.
I2S_TransferAbortDMA() function aborts transmit or receive operation in DMA mode.
Length of buffer for transmit or receive has to be multiply of 4 bytes. Buffer address has to be aligned to 4-bytes. Data are put into or taken from FIFO unaltered in DMA mode so buffer has to be prepared according to following information.
If i2s_config_t.dataLength (channel bit width) is between 4 and 16, every word in buffer should contain data for left and right channels.
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R15   | R14   | R13   | R12   | R11   | R10   | R09   | R08   | R07   | R06   | R05   | R04   | R03   | R02   | R01   | R00   | L15   | L14   | L13   | L12   | L11   | L10   | L09   | L08   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
Rnn - right channel bit nn 
Lnn - left channel bit nn 
 Note that for example if i2s_config_t.dataLength = 7, bits on positions R07-R15 and L07-L15 are ignored (buffer "wastes space"). 
If i2s_config_t.dataLength (channel bit width) is between 17 and 24 and i2s_config_t.pack48 = false:
Even words (counting from zero):
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
L23   | L22   | L21   | L20   | L19   | L18   | L17   | L16   | L15   | L14   | L13   | L12   | L11   | L10   | L09   | L08   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
Odd words (counting from zero):
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R23   | R22   | R21   | R20   | R19   | R18   | R17   | R16   | R15   | R14   | R13   | R12   | R11   | R10   | R09   | R08   | R07   | R06   | R05   | R04   | R03   | R02   | R01   | R00    | 
If i2s_config_t.dataLength (channel bit width) is between 17 and 24 and i2s_config_t.pack48 = true:
Even words (counting from zero):
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R07   | R06   | R05   | R04   | R03   | R02   | R01   | R00   | L23   | L22   | L21   | L20   | L19   | L18   | L17   | L16   | L15   | L14   | L13   | L12   | L11   | L10   | L09   | L08   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
Odd words (counting from zero):
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R23   | R22   | R21   | R20   | R19   | R18   | R17   | R16   | R15   | R14   | R13   | R12   | R11   | R10   | R09   | R08    | 
If i2s_config_t.dataLength (channel bit width) is between 25 and 32:
Even words (counting from zero):
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
L31   | L30   | L29   | L28   | L27   | L26   | L25   | L24   | L23   | L22   | L21   | L20   | L19   | L18   | L17   | L16   | L15   | L14   | L13   | L12   | L11   | L10   | L09   | L08   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
Odd words (counting from zero):
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R31   | R30   | R29   | R28   | R27   | R26   | R25   | R24   | R23   | R22   | R21   | R20   | R19   | R18   | R17   | R16   | R15   | R14   | R13   | R12   | R11   | R10   | R09   | R08   | R07   | R06   | R05   | R04   | R03   | R02   | R01   | R00    | 
If i2s_config_t.dataLength (channel bit width) is 4:
Buffer does not need to be aligned (buffer is read / written by single bytes, each byte contain left and right channel):
MSB   | LSB    | ||||||
|---|---|---|---|---|---|---|---|
R03   | R02   | R01   | R00   | L03   | L02   | L01   | L00    | 
If i2s_config_t.dataLength (channel bit width) is between 5 and 8:
Length of buffer for transmit or receive has to be multiply of 2 bytes. Buffer address has to be aligned to 2-bytes.
MSB   | LSB    | ||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R07   | R06   | R05   | R04   | R03   | R02   | R01   | R00   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
If i2s_config_t.dataLength (channel bit width) is between 9 and 16:
Length of buffer for transmit or receive has to be multiply of 4 bytes. Buffer address has to be aligned to 4-bytes.
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R15   | R14   | R13   | R12   | R11   | R10   | R09   | R08   | R07   | R06   | R05   | R04   | R03   | R02   | R01   | R00   | L15   | L14   | L13   | L12   | L11   | L10   | L09   | L08   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
If i2s_config_t.dataLength (channel bit width) is between 17 and 24 and i2s_config_t.pack48 = false:
Length of buffer for transmit or receive has to be multiply of 6 bytes.
MSB   | LSB    | ||||||||||||||||||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R23   | R22   | R21   | R20   | R19   | R18   | R17   | R16   | R15   | R14   | R13   | R12   | R11   | R10   | R09   | R08   | R07   | R06   | R05   | R04   | R03   | R02   | R01   | R00   | L23   | L22   | L21   | L20   | L19   | L18   | L17   | L16   | L15   | L14   | L13   | L12   | L11   | L10   | L09   | L08   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
If i2s_config_t.dataLength (channel bit width) is between 17 and 24 and i2s_config_t.pack48 = true:
Length of buffer for transmit or receive has to be multiply of 6 bytes. Buffer address has to be aligned to 4-bytes.
MSB   | LSB    | ||||||||||||||||||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R23   | R22   | R21   | R20   | R19   | R18   | R17   | R16   | R15   | R14   | R13   | R12   | R11   | R10   | R09   | R08   | R07   | R06   | R05   | R04   | R03   | R02   | R01   | R00   | L23   | L22   | L21   | L20   | L19   | L18   | L17   | L16   | L15   | L14   | L13   | L12   | L11   | L10   | L09   | L08   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
If i2s_config_t.dataLength (channel bit width) is between 25 and 32 and i2s_config_t.oneChannel = false:
Buffer for transmit or receive has to be multiply of 8 bytes. Buffer address has to be aligned to 4-bytes.
Even words (counting from zero):
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
L31   | L30   | L29   | L28   | L27   | L26   | L25   | L24   | L23   | L22   | L21   | L20   | L19   | L18   | L17   | L16   | L15   | L14   | L13   | L12   | L11   | L10   | L09   | L08   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
Odd words (counting from zero):
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
R31   | R30   | R29   | R28   | R27   | R26   | R25   | R24   | R23   | R22   | R21   | R20   | R19   | R18   | R17   | R16   | R15   | R14   | R13   | R12   | R11   | R10   | R09   | R08   | R07   | R06   | R05   | R04   | R03   | R02   | R01   | R00    | 
If i2s_config_t.dataLength (channel bit width) is between 25 and 32 and i2s_config_t.oneChannel = true:
Buffer for transmit or receive has to be multiply of 4 bytes. Buffer address has to be aligned to 4-bytes.
MSB   | LSB    | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
L31   | L30   | L29   | L28   | L27   | L26   | L25   | L24   | L23   | L22   | L21   | L20   | L19   | L18   | L17   | L16   | L15   | L14   | L13   | L12   | L11   | L10   | L09   | L08   | L07   | L06   | L05   | L04   | L03   | L02   | L01   | L00    | 
Transmit example
Receive example
Transmit example
Receive example
Modules | |
| I2S DMA Driver | |
| I2S Driver | |