| ► examples | |
| ► platform | |
| mcuxCl_clns.h | CLNS header for component-independent functionality |
| mcuxClAead.h | Top-level include file for the mcuxClAead component |
| mcuxClAead_Constants.h | Constants for use with the mcuxClAead component |
| mcuxClAead_Functions.h | Top-level API of the mcuxClAead component |
| mcuxClAead_Types.h | Type definitions for the mcuxClAead component |
| mcuxClAeadModes.h | |
| mcuxClAeadModes_Modes.h | This file defines the modes for the mcuxClAeadModes component |
| mcuxClAes.h | Top-level interface header for the mcuxClAes component |
| mcuxClAes_Constants.h | |
| mcuxClAes_KeyTypes.h | Definition of supported key types in mcuxClAes component, see also mcuxClKey component |
| mcuxClAes_Types.h | Type definitions for the mcuxClAes component |
| mcuxClBuffer.h | Provides the API for the CL buffer types |
| mcuxClBuffer_Cfg.h | Configuration of the implementation for the buffer types |
| mcuxClBuffer_Constants.h | Constants for use with the mcuxClBuffer component |
| mcuxClBuffer_Impl.h | Selection of the implementation for the buffer types |
| mcuxClBuffer_Pointer.h | Provides the implementation for the basic C pointer buffer types |
| mcuxClCipher.h | Top-level include file for the mcuxClCipher component |
| mcuxClCipher_Constants.h | Constants for use with the mcuxClCipher component |
| mcuxClCipher_Functions.h | Top-level API of the mcuxClCipher component |
| mcuxClCipher_Types.h | Type definitions for the mcuxClCipher component |
| mcuxClCipherModes.h | |
| mcuxClCipherModes_Modes.h | Supported modes for the mcuxClCipher component |
| mcuxClCore_Examples.h | |
| mcuxClCore_FunctionIdentifiers.h | Definition of function identifiers for the flow protection mechanism |
| mcuxClCore_Macros.h | Definition of macros |
| mcuxClCore_Platform.h | |
| mcuxClCore_Toolchain.h | |
| mcuxClEcc.h | Top level header of mcuxClEcc component |
| mcuxClEcc_Constants.h | Constant definitions of mcuxClEcc component |
| mcuxClEcc_Functions.h | Top level APIs of mcuxClEcc component |
| mcuxClEcc_KeyTypes.h | ECC related definitions to be used for key handling mechanisms of the mcuxClKey component |
| mcuxClEcc_Types.h | Type definitions and descriptors of mcuxClEcc component |
| mcuxClEls.h | Top-level include file for the ELS driver |
| mcuxClEls_Aead.h | ELS header for Authenticated Encryption with Associated Data (AEAD) |
| mcuxClEls_Cipher.h | ELS header for symmetric ciphers |
| mcuxClEls_Cmac.h | ELS header for CMAC support |
| mcuxClEls_Common.h | ELS header for common functionality |
| mcuxClEls_Ecc.h | ELS header for elliptic curve cryptography This header exposes functions that enable using the ELS for elliptic curve cryptography |
| mcuxClEls_Hash.h | ELS header for hashing |
| mcuxClEls_Hmac.h | ELS header for HMAC support |
| mcuxClEls_Kdf.h | ELS header for key derivation |
| mcuxClEls_KeyManagement.h | ELS header for key management |
| mcuxClEls_mapping.h | Header providing mapping for legacy function/definition names (with CSS) |
| mcuxClEls_Rng.h | ELS header for random number generation |
| mcuxClEls_Types.h | ELS type header |
| mcuxClExample_ELS_Helper.h | |
| mcuxClExample_ELS_Key_Helper.h | |
| mcuxClExample_Key_Helper.h | |
| mcuxClExample_RFC3394_Helper.h | |
| mcuxClExample_RNG_Helper.h | |
| mcuxClExample_Session_Helper.h | |
| mcuxClHash.h | Top-level include file for the mcuxClHash component |
| mcuxClHash_Constants.h | Constants for use with the mcuxClHash component |
| mcuxClHash_Functions.h | Top-level API of the mcuxClHash component |
| mcuxClHash_Types.h | Type definitions for the mcuxClHash component |
| mcuxClHashModes.h | |
| mcuxClHashModes_Algorithms.h | Algorithm/mode definitions for the mcuxClHashModes component |
| mcuxClHashModes_Constants.h | Constants for use with the mcuxClHashModes component |
| mcuxClHashModes_Functions.h | |
| mcuxClHmac.h | |
| mcuxClHmac_Constants.h | Constants for the mcuxClHmac component |
| mcuxClHmac_Functions.h | Functions for the mcuxClHmac component |
| mcuxClHmac_KeyTypes.h | Definition of supported key types in mcuxClHmac component, see also mcuxClKey component |
| mcuxClHmac_Modes.h | Mode descriptors for the mcuxClHmac component |
| mcuxClKey.h | Top-level include file for the mcuxClKey component |
| mcuxClKey_Constants.h | Constants for the mcuxClKey component |
| mcuxClKey_Functions.h | Top-level API of the mcuxClKey component |
| mcuxClKey_ProtectionMechanisms.h | |
| mcuxClKey_Types.h | Type definitions for the mcuxClKey component |
| mcuxClMac.h | Top-level include file for the mcuxClMac component |
| mcuxClMac_Constants.h | Constants and status codes for the mcuxClMac component |
| mcuxClMac_Functions.h | Top-level API of the mcuxClMac component |
| mcuxClMac_Types.h | Type definitions for the mcuxClMac component |
| mcuxClMacModes.h | |
| mcuxClMacModes_Constants.h | Constants for the mcuxClMacModes component |
| mcuxClMacModes_Functions.h | Functions for the mcuxClMacModes component |
| mcuxClMacModes_Modes.h | |
| mcuxClMath.h | Top level header of mcuxClMath component |
| mcuxClMath_Functions.h | APIs of mcuxClMath component |
| mcuxClMath_Types.h | |
| mcuxClMemory.h | Top-level include file for the memory operations |
| mcuxClMemory_Clear.h | Memory header for clear functions |
| mcuxClMemory_Constants.h | Memory constant header |
| mcuxClMemory_Copy.h | Memory header for copy functions |
| mcuxClMemory_Copy_Reversed.h | Memory header for reversed copy functions |
| mcuxClMemory_Endianness.h | Memory header for endianness support functions |
| mcuxClMemory_Set.h | Memory header for set function |
| mcuxClMemory_Types.h | Memory type header |
| mcuxClMemory_Xor.h | Memory header for xor functions |
| mcuxClPadding.h | Top-level include file for the padding component |
| mcuxClPadding_Constants.h | Constants definitions for the mcuxClPadding component |
| mcuxClPadding_Types.h | Type definitions for the mcuxClPadding component |
| mcuxClPkc.h | Top level header of mcuxClPkc component (PKC hardware driver) |
| mcuxClPkc_Functions.h | APIs of mcuxClPkc component |
| mcuxClPkc_Types.h | Type definitions of mcuxClPkc component |
| mcuxClRandom.h | Top level header of mcuxClRandom component |
| mcuxClRandom_Constants.h | Constant definitions of mcuxClRandom component |
| mcuxClRandom_Functions.h | Top level APIs of mcuxClRandom component |
| mcuxClRandom_Types.h | Type definitions of mcuxClRandom component |
| mcuxClRandomModes.h | Top level header of mcuxClRandomModes component |
| mcuxClRandomModes_Constants.h | Mode definitions of mcuxClRandomModes component |
| mcuxClRandomModes_Functions_PatchMode.h | |
| mcuxClRsa.h | Top-level include file for the mcuxClRsa component |
| mcuxClRsa_Constants.h | Constant definitions for the mcuxClRsa component |
| mcuxClRsa_Functions.h | Top-level API of the mcuxClRsa component |
| mcuxClRsa_Types.h | Type definitions for the mcuxClRsa component |
| mcuxClSession.h | Top-level include file for the mcuxClSession component |
| mcuxClSession_Functions.h | Top-level API of the mcuxClSession component |
| mcuxClSession_Types.h | Type definitions for the mcuxClSession component |
| mcuxCsslAnalysis.h | |
| mcuxCsslCPreProcessor.h | The default implementation is based on standard C preprocessor functionality |
| mcuxCsslDataIntegrity.h | Provides the API for the CSSL data integrity mechanism |
| mcuxCsslDataIntegrity_Cfg.h | Configuration of the implementation for the data integrity mechanism |
| mcuxCsslDataIntegrity_Impl.h | Selection of the implementation for the data integrity mechanism |
| mcuxCsslDataIntegrity_None.h | Implementation that disables the CSSL data integrity mechanism |
| mcuxCsslFlowProtection.h | Provides the API for the CSSL flow protection mechanism |
| mcuxCsslFlowProtection_Cfg.h | Configuration of the implementation for the flow protection mechanism |
| mcuxCsslFlowProtection_FunctionIdentifiers.h | Definition of function identifiers for the flow protection mechanism |
| mcuxCsslFlowProtection_Impl.h | Selection of the implementation for the flow protection mechanism |
| mcuxCsslFlowProtection_SecureCounter_Common.h | Counter based implementation for the flow protection mechanism, for a local security counter |
| mcuxCsslFlowProtection_SecureCounter_Local.h | Counter based implementation for the flow protection mechanism, for a local security counter |
| mcuxCsslMemory.h | Top-level include file for the CSSL memory functions |
| mcuxCsslMemory_Clear.h | Header file of memory clear function |
| mcuxCsslMemory_Compare.h | Include file for constant time memory compare function |
| mcuxCsslMemory_Constants.h | Constants definitions for the mcuxCsslMemory component |
| mcuxCsslMemory_Copy.h | Include file for memory copy function |
| mcuxCsslMemory_Set.h | Header file of memory set function |
| mcuxCsslMemory_Types.h | Type definitions for the mcuxCsslMemory component |
| mcuxCsslParamIntegrity.h | Top-level include file for the parameter integrity protection mechanism |
| mcuxCsslSecureCounter.h | Provides the API for the CSSL secure counter mechanism |
| mcuxCsslSecureCounter_Cfg.h | Configuration of the implementation for the secure counter mechanism |
| mcuxCsslSecureCounter_Impl.h | Selection of the implementation for the secure counter mechanism |
| mcuxCsslSecureCounter_None.h | Implementation that disables the CSSL secure counter mechanism |
| mcuxCsslSecureCounter_SW_Local.h | SW implementation of the CSSL secure counter mechanism (using a local variable) |