MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslMemory_Examples.h
1/*--------------------------------------------------------------------------*/
2/* Copyright 2023-2025 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
14#ifndef MCUXCSSLMEMORY_EXAMPLES_H_
15#define MCUXCSSLMEMORY_EXAMPLES_H_
16
17#include <stdint.h>
18#include <stdbool.h>
19#include <stddef.h>
20
21#define MCUXCSSL_MEMORY_EX_FUNCTION(_name) __attribute__((section(".example"))) bool _name(void)
22
23#define MCUXCSSLMEMORY_EX_OK true
24#define MCUXCSSLMEMORY_EX_ERROR false
25
26MCUXCSSL_MEMORY_EX_FUNCTION(mcuxCsslMemory_Compare_example);
27MCUXCSSL_MEMORY_EX_FUNCTION(mcuxCsslMemory_Copy_example);
28MCUXCSSL_MEMORY_EX_FUNCTION(mcuxCsslMemory_Clear_example);
29MCUXCSSL_MEMORY_EX_FUNCTION(mcuxCsslMemory_Set_example);
30MCUXCSSL_MEMORY_EX_FUNCTION(mcuxCsslMemory_SecureSet_example);
31
32#endif /* MCUXCSSLMEMORY_EXAMPLES_H_ */