MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClAead_Functions.h File Reference

Top-level API of the mcuxClAead component. More...

#include <mcuxClConfig.h>
#include <mcuxClSession_Types.h>
#include <mcuxClKey.h>
#include <mcuxClAead_Types.h>
#include <mcuxClBuffer.h>

Go to the source code of this file.

Functions

mcuxClAead_Status_t mcuxClAead_encrypt (mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClAead_Mode_t mode, mcuxCl_InputBuffer_t pNonce, uint32_t nonceLength, mcuxCl_InputBuffer_t pIn, uint32_t inLength, mcuxCl_InputBuffer_t pAdata, uint32_t adataLength, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength, mcuxCl_Buffer_t pTag, uint32_t tagLength)
 One-shot authenticated encryption function.
mcuxClAead_Status_t mcuxClAead_decrypt (mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClAead_Mode_t mode, mcuxCl_InputBuffer_t pNonce, uint32_t nonceLength, mcuxCl_InputBuffer_t pIn, uint32_t inLength, mcuxCl_InputBuffer_t pAdata, uint32_t adataLength, mcuxCl_InputBuffer_t pTag, uint32_t tagLength, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
 One-shot authenticated decryption function.
mcuxClAead_Status_t mcuxClAead_init_encrypt (mcuxClSession_Handle_t session, mcuxClAead_Context_t *const pContext, mcuxClKey_Handle_t key, mcuxClAead_Mode_t mode, mcuxCl_InputBuffer_t pNonce, uint32_t nonceLength, uint32_t inLength, uint32_t adataLength, uint32_t tagLength)
 Multi-part authenticated encryption initialization function.
mcuxClAead_Status_t mcuxClAead_init_decrypt (mcuxClSession_Handle_t session, mcuxClAead_Context_t *const pContext, mcuxClKey_Handle_t key, mcuxClAead_Mode_t mode, mcuxCl_InputBuffer_t pNonce, uint32_t nonceLength, uint32_t inLength, uint32_t adataLength, uint32_t tagLength)
 Multi-part authenticated decryption initialization function.
mcuxClAead_Status_t mcuxClAead_process (mcuxClSession_Handle_t session, mcuxClAead_Context_t *const pContext, mcuxCl_InputBuffer_t pIn, uint32_t inLength, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
 Multi-part authenticated encryption/decryption processing function for the regular data (authenticated and encrypted).
mcuxClAead_Status_t mcuxClAead_process_adata (mcuxClSession_Handle_t session, mcuxClAead_Context_t *const pContext, mcuxCl_InputBuffer_t pAdata, uint32_t adataLength)
 Multi-part authenticated encryption/decryption processing function for the associated data (authenticated only).
mcuxClAead_Status_t mcuxClAead_finish (mcuxClSession_Handle_t session, mcuxClAead_Context_t *const pContext, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength, mcuxCl_Buffer_t pTag)
 Multi-part authenticated encryption/decryption finalization function.
mcuxClAead_Status_t mcuxClAead_verify (mcuxClSession_Handle_t session, mcuxClAead_Context_t *const pContext, mcuxCl_InputBuffer_t pTag, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
 Multi-part authenticated decryption verification function.

Detailed Description

Top-level API of the mcuxClAead component.