MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClAes.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2022 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
23
24#ifndef MCUXCLAES_H_
25#define MCUXCLAES_H_
26
27#include <mcuxClConfig.h> // Exported features flags header
28
29#include <mcuxClAes_Constants.h>
30#include <mcuxClAes_KeyTypes.h>
31#include <mcuxClAes_Types.h>
33#endif /* MCUXCLAES_H_ */
Definition of internal key types in mcuxClAes component.
Definition of supported key types in mcuxClAes component, see also mcuxClKey component.
Type definitions for the mcuxClAes component.