MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClBuffer_Impl.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2022-2023 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19#ifndef MCUXCLBUFFER_IMPL_H_
20#define MCUXCLBUFFER_IMPL_H_
21
22#include <mcuxClCore_Platform.h>
23
24/* Include the configuration for the buffer types. */
25#include <mcuxClBuffer_Cfg.h>
26
27/* Include the selected implementation of the buffer types. */
28#if defined(MCUXCLBUFFER_USE_OBJECT) && (1 == MCUXCLBUFFER_USE_OBJECT)
29# include <mcuxClBuffer_Object.h>
30#elif defined(MCUXCLBUFFER_USE_POINTER) && (1 == MCUXCLBUFFER_USE_POINTER)
31# include <mcuxClBuffer_Pointer.h>
32#else
33# error "No buffer type implementation found/configured."
34#endif
35
36#endif /* MCUXCLBUFFER_IMPL_H_ */
Configuration of the implementation for the buffer types.
Provides the implementation for the basic C pointer buffer types.