MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClCipher_Types.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2023 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
17
18#ifndef MCUXCLCIPHER_TYPES_H_
19#define MCUXCLCIPHER_TYPES_H_
20
21#include <stdint.h>
22#include <stdbool.h>
23#include <stddef.h>
24
25#include <mcuxClConfig.h> // Exported features flags header
26#include <mcuxClSession.h>
27
28
29#ifdef __cplusplus
30extern "C" {
31#endif
32
39
46struct mcuxClCipher_ModeDescriptor;
47
54typedef struct mcuxClCipher_ModeDescriptor mcuxClCipher_ModeDescriptor_t;
55
62
69struct mcuxClCipher_TestDescriptor;
70
77typedef struct mcuxClCipher_TestDescriptor mcuxClCipher_TestDescriptor_t;
78
85
92struct mcuxClCipher_Context;
93
100typedef struct mcuxClCipher_Context mcuxClCipher_Context_t;
101
108typedef uint32_t mcuxClCipher_Status_t;
109
111
112#ifdef __cplusplus
113} /* extern "C" */
114#endif
115
116#endif /* MCUXCLCIPHER_TYPES_H_ */
Top-level include file for the mcuxClSession component.
const mcuxClCipher_TestDescriptor_t *const mcuxClCipher_Test_t
Cipher selftest mode/algorithm type.
Definition mcuxClCipher_Types.h:84
struct mcuxClCipher_Context mcuxClCipher_Context_t
Cipher context type.
Definition mcuxClCipher_Types.h:100
struct mcuxClCipher_ModeDescriptor mcuxClCipher_ModeDescriptor_t
Cipher mode/algorithm descriptor type.
Definition mcuxClCipher_Types.h:54
const mcuxClCipher_ModeDescriptor_t *const mcuxClCipher_Mode_t
Cipher mode/algorithm type.
Definition mcuxClCipher_Types.h:61
uint32_t mcuxClCipher_Status_t
Cipher status code.
Definition mcuxClCipher_Types.h:108
struct mcuxClCipher_TestDescriptor mcuxClCipher_TestDescriptor_t
Cipher selftest mode/algorithm descriptor type.
Definition mcuxClCipher_Types.h:77