MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClDma_Types.h File Reference

Type and associated constant definitions of the mcuxClDma component. More...

#include <mcuxClCore_Platform.h>

Go to the source code of this file.

Macros

#define MCUXCLDMA_STATUS_SOURCE_BUS_ERROR
 Source address bus is not accessible by DMA.
#define MCUXCLDMA_STATUS_DESTINATION_BUS_ERROR
 Destination address bus is not accessible by DMA.
#define MCUXCLDMA_STATUS_CONFIGURATION_ERROR
 DMA was not correctly configured.
#define MCUXCLDMA_STATUS_OK
 No error occurred.

Typedefs

typedef uint32_t mcuxClDma_Status_t
 DMA status code.

Detailed Description

Type and associated constant definitions of the mcuxClDma component.