MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClEcc.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2024 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
21
22
23#ifndef MCUXCLECC_H_
24#define MCUXCLECC_H_
25
26#include <mcuxClCore_Platform.h>
27#include <mcuxClEcc_Types.h>
28#include <mcuxClEcc_Constants.h>
29#include <mcuxClEcc_Functions.h>
32#include <mcuxClEcc_KeyTypes.h>
33
34
35
36#endif /* MCUXCLECC_H_ */
Constant definitions of mcuxClEcc component.
Top level APIs of mcuxClEcc component.
Definition of internal key types in mcuxClEcc component.
ECC related definitions to be used for key handling mechanisms of the mcuxClKey component.
Type definitions and descriptors of mcuxClEcc component.
Defines the memory consumption for the mcuxClEcc component.