20#ifndef MCUXCLFFDH_TYPES_H_
21#define MCUXCLFFDH_TYPES_H_
24#include <mcuxClCore_Platform.h>
27#include <mcuxCsslAnalysis.h>
Top-level include file for the mcuxClBuffer component.
Constant definitions of mcuxClFfdh component.
Provides the API for the CSSL flow protection mechanism.
struct mcuxClFfdh_DomainParams mcuxClFfdh_DomainParams_t
Type for FFDH domain parameters.
Definition mcuxClFfdh_Types.h:47
uint32_t mcuxClFfdh_Status_t
Type for mcuxClFfdh component return codes.
Definition mcuxClFfdh_Types.h:44