MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClHash.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2023 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
42
43#ifndef MCUXCLHASH_H_
44#define MCUXCLHASH_H_
45
46#include <mcuxClConfig.h> // Exported features flags header
47#include <mcuxClHash_Types.h>
51
52#endif /* MCUXCLHASH_H_ */
Constants for use with the mcuxClHash component.
Top-level API of the mcuxClHash component.
Type definitions for the mcuxClHash component.
Defines the memory consumption for the mcuxClHash component.