MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClHash_Types.h File Reference

Type definitions for the mcuxClHash component. More...

#include <mcuxClConfig.h>
#include <mcuxClCore_Platform.h>

Go to the source code of this file.

Typedefs

typedef struct mcuxClHash_AlgorithmDescriptor mcuxClHash_AlgorithmDescriptor_t
 Hash mode/algorithm descriptor type.
typedef const mcuxClHash_AlgorithmDescriptor_t *const mcuxClHash_Algo_t
 Hash mode/algorithm type.
typedef struct mcuxClHash_ContextDescriptor mcuxClHash_ContextDescriptor_t
 Hash Context buffer type.
typedef mcuxClHash_ContextDescriptor_tmcuxClHash_Context_t
 Hash Context type.
typedef uint32_t mcuxClHash_Status_t
 Hash Status type.

Detailed Description

Type definitions for the mcuxClHash component.