MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClMacModes_Functions.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2022-2025 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19#ifndef MCUXCLMACMODES_FUNCTIONS_H_
20#define MCUXCLMACMODES_FUNCTIONS_H_
21
23#include <mcuxClSession_Types.h>
24#include <mcuxClKey_Types.h>
25#include <mcuxClMac_Types.h>
26#include <mcuxClCore_Platform.h>
27#include <mcuxClBuffer.h>
28
29#ifdef __cplusplus
30extern "C" {
31#endif
32
39
46
47 /* mcuxClMacModes_Constructors */
51 /* mcuxClMacModes_Functions */
55
56#ifdef __cplusplus
57} /* extern "C" */
58#endif
59
60#endif /* MCUXCLMACMODES_FUNCTIONS_H_ */
Top-level include file for the mcuxClBuffer component.
Type definitions for the mcuxClKey component.
Type definitions for the mcuxClMac component.
Type definitions for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.