MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClMac_Types.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2024 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
17
18#ifndef MCUXCLMAC_TYPES_H_
19#define MCUXCLMAC_TYPES_H_
20
21#include <stdint.h>
22#include <stdbool.h>
23#include <stddef.h>
24
25#include <mcuxClConfig.h> // Exported features flags header
26#include <mcuxClSession_Types.h>
29
36
37/**********************************************
38 * TYPEDEFS
39 **********************************************/
40
44typedef uint32_t mcuxClMac_Status_t;
45
52struct mcuxClMac_ModeDescriptor;
53
60typedef struct mcuxClMac_ModeDescriptor mcuxClMac_ModeDescriptor_t;
61
68
76
77
84struct mcuxClMac_Context;
85
98typedef struct mcuxClMac_Context mcuxClMac_Context_t;
99 /* mcuxClMac_Types */
103
104#endif /* MCUXCLMAC_TYPES_H_ */
Definition of function identifiers for the flow protection mechanism.
Type definitions for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
mcuxClMac_ModeDescriptor_t *const mcuxClMac_CustomMode_t
MAC custom mode/algorithm type.
Definition mcuxClMac_Types.h:75
const mcuxClMac_ModeDescriptor_t *const mcuxClMac_Mode_t
MAC mode/algorithm type.
Definition mcuxClMac_Types.h:67
struct mcuxClMac_ModeDescriptor mcuxClMac_ModeDescriptor_t
MAC mode/algorithm descriptor type.
Definition mcuxClMac_Types.h:60
uint32_t mcuxClMac_Status_t
Type for Mac component error codes.
Definition mcuxClMac_Types.h:44
struct mcuxClMac_Context mcuxClMac_Context_t
Mac context type.
Definition mcuxClMac_Types.h:98