MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClMemory.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2021, 2023 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
25
26#ifndef MCUXCLMEMORY_H
27#define MCUXCLMEMORY_H
28
29#include <mcuxClConfig.h> // Exported features flags header
33#include <mcuxClMemory_Types.h>
35#include <mcuxClMemory_Clear.h>
36#include <mcuxClMemory_Copy.h>
38#include <mcuxClMemory_Set.h>
39#include <mcuxClMemory_Xor.h>
40
44#endif
Definition of function identifiers for the flow protection mechanism.
Memory header for clear functions.
Memory constant header.
Memory header for copy functions.
Memory header for reversed copy functions.
Memory header for endianness support functions.
Memory header for set function.
Memory type header.
Memory header for xor functions.
Provides the API for the CSSL flow protection mechanism.