MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClMemory_Constants.h File Reference

Memory constant header. More...

Go to the source code of this file.

Macros

#define MCUXCLMEMORY_COMPONENT_MASK
 Component mask value.
#define MCUXCLMEMORY_STATUS_EQUAL
 The two contents of the Memory Compare are equal.
#define MCUXCLMEMORY_STATUS_NOT_EQUAL
 The two contents of the Memory Compare are not equal.
#define MCUXCLMEMORY_STATUS_FAULT
 A fault occurred in the execution.

Detailed Description

Memory constant header.

This header exposes constants used by the mcuxClMemory functions.